Hi.
It is a question about "OMX.TI.VPSSM3.VFPC.NF".
Does the modular setting method have a difference
between "ti-ezsdk_dm816x-evm_5_03_01_15/omx_05_02_00_30"
and "ti-ezsdk_dm816x-evm_5_04_00_11/omx_05_02_00_38"?
Where is databook for the configuration parameter of NF module?
-------
NF module was used using ti-ezsdk_dm816x-evm_5_03_01_15/omx_05_02_00_30.
This operated appropriately.
It was made to operate by ti-ezsdk_dm816x-evm_5_04_00_11/omx_05_02_00_38 with the same sauce.
But, It becomes an instruction-execution-time error and does not operate.
It will become the error of OMX_EventError:OMX_ErrorInsufficientResources (0x80001000)
at OMX_SendCommand (Client->pNfHandle, OMX_CommandStateSet, OMX_StateIdle, NULL);
Regards,
Miki Shinji