Other Parts Discussed in Thread: TWL6030
Hi,
I am running ICS with Pandaboard (OMAP4430).
I have downloaded release software from "http://omappedia.org/wiki/4AI.1.4_OMAP4_Icecream_Sandwich_Panda_Notes"
My SD card having two partition 1.boot and 2.rootfs
I am not using fastboot for partitioning and flashing my device.
After successful boot i am getting "Encryption Unsuccessful" "Reset Phone" message on my display.
To resolve this issue i have tried to change encryption feature from "system/core/init/builtins.c" file by disabling encryption.
Here given below is the modification in "system/core/init/builtins.c" file
========================================================================
In do_mount()
- property_set("ro.crypto.state","encrypted");
+ property_set("ro.crypto.state","unencrypted");
- property_set("vold.decrypt",1);
========================================================================
Using this new rootfs i am still getting the same error.
The log I am getting is :
========================================================================
Texas Instruments X-Loader 1.5.1 (Aug 23 2012 - 15:43:54)
Reading boot sector
Loading u-boot.bin from mmc
U-Boot 2012.04.01 (Aug 23 2012 - 15:44:35)
CPU : OMAP4430 ES2.1
Board: OMAP4 Panda
I2C: ready
DRAM: 1 GiB
MMC: OMAP SD/MMC: 0
Using default environment
In: serial
Out: serial
Err: serial
Net: No ethernet found.
checking for preEnv.txt
reading preEnv.txt
** Unable to read "preEnv.txt" from mmc 0:1 **
Hit any key to stop autoboot: 3 2 1 0
reading uEnv.txt
** Unable to read "uEnv.txt" from mmc 0:1 **
reading boot.scr
386 bytes read
Loaded script from boot.scr
Running bootscript from mmc0 ...
## Executing script at 82000000
(Re)start USB...
USB: Register 1313 NbrPorts 3
USB EHCI 1.00
scanning bus for devices... 4 USB Device(s) found
scanning bus for storage devices... 0 Storage Device(s) found
scanning bus for ethernet devices... 1 Ethernet Device(s) found
Waiting for Ethernet connection... done.
BOOTP broadcast 1
DHCP client bound to address 10.99.15.19
Using sms0 device
TFTP from server 192.168.6.59; our IP address is 10.99.15.19; sending through gateway 10.99.13.1
Filename 'pxelinux.0'.
Load address: 0x82000000
Loading: *##
done
Bytes transferred = 14776 (39b8 hex)
Waiting for Ethernet connection... done.
Using sms0 device
TFTP from server 10.99.14.184; our IP address is 10.99.15.19
Filename 'brijesh/pandaboard/uImage'.
Load address: 0x80c00000
Loading: *#################################################################
#################################################################
#################################################################
#################################################################
##########################
done
Bytes transferred = 4190056 (3fef68 hex)
## Booting kernel from Legacy Image at 80c00000 ...
Image Name: Linux-3.0.21-00003-OMAP-Android+
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4189992 Bytes = 4 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Linux version 3.0.21-00003-OMAP-Android+ (root@EICPU) (gcc version 4.4.1 (Sourcery G++ Lite 2010q1-202) ) #3 SMP PREEMPT Wed Aug 29 16:47:13 IST 2012
[ 0.000000] CPU: ARMv7 Processor [411fc092] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: OMAP4 Panda board
[ 0.000000] Truncating RAM at 80000000-bfffffff to -afffffff (vmalloc region overlap).
[ 0.000000] Truncating RAM at a0000000-bfffffff to -afffffff (vmalloc region overlap).
[ 0.000000] Reserving 33554432 bytes SDRAM for VRAM
[ 0.000000] Memory policy: ECC disabled, Data cache writealloc
[ 0.000000] OMAP4430 ES2.1
[ 0.000000] SRAM: Mapped pa 0x40300000 to va 0xfe400000 size: 0xd000
[ 0.000000] On node 0 totalpages: 169984
[ 0.000000] free_area_init_node: node 0, pgdat c08130e0, node_mem_map c0962000
[ 0.000000] Normal zone: 1536 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 168448 pages, LIFO batch:31
[ 0.000000] powerdomain: waited too long for powerdomain dss_pwrdm to complete transition
[ 0.000000] PERCPU: Embedded 7 pages/cpu @c0f6c000 s6912 r8192 d13568 u32768
[ 0.000000] pcpu-alloc: s6912 r8192 d13568 u32768 alloc=8*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 168448
[ 0.000000] Kernel command line: console=ttyO2,115200n8 mem=1G androidboot.console=ttyO2 console=ttyO2,115200n8 androidboot.console=ttyO2 mem=456M@0x80000000 mem=512M@0xA0000000 root=/dev/mmcblk0p2 rw rootdelay=2 init=/init vram="32M" omapfb.vram=0:16M,1:16M consoleblank=0
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 512MB 152MB = 664MB total
[ 0.000000] Memory: 663296k/1269248k available, 246272k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
[ 0.000000] vmalloc : 0xf0800000 - 0xf8000000 ( 120 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .init : 0xc0008000 - 0xc004c000 ( 272 kB)
[ 0.000000] .text : 0xc004c000 - 0xc07aa000 (7544 kB)
[ 0.000000] .data : 0xc07aa000 - 0xc08138c0 ( 423 kB)
[ 0.000000] .bss : 0xc08138e4 - 0xc0961460 (1335 kB)
[ 0.000000] SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] NR_IRQS:410
[ 0.000000] omap_hwmod: dpll_mpu_m2_ck: missing clockdomain for dpll_mpu_m2_ck.
[ 0.000000] OMAP clockevent source: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000061] Calibrating delay loop... 2007.19 BogoMIPS (lpj=7839744)
[ 0.015716] pid_max: default: 32768 minimum: 301
[ 0.015716] Mount-cache hash table entries: 512
[ 0.071411] Initializing cgroup subsys debug
[ 0.071441] Initializing cgroup subsys cpuacct
[ 0.071441] Initializing cgroup subsys freezer
[ 0.071533] CPU: Testing write buffer coherency: ok
[ 0.072021] L310 cache controller enabled
[ 0.072052] l2x0: 16 ways, CACHE_ID 0x410000c4, AUX_CTRL 0x5e470000, Cache size: 1048576 B
[ 0.150451] CPU1: Booted secondary processor
[ 0.220520] Brought up 2 CPUs
[ 0.220520] SMP: Total of 2 processors activated (4022.78 BogoMIPS).
[ 0.220703] devtmpfs: initialized
[ 0.220855] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for emif_fw
[ 0.223114] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l3_instr
[ 0.223114] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l3_main_1
[ 0.223114] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l3_main_2
[ 0.223144] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l4_abe
[ 0.223144] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l4_cfg
[ 0.223144] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l4_per
[ 0.223175] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l4_wkup
[ 0.223175] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for mpu_private
[ 0.223175] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for sl2if
[ 0.223266] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for usbhs_ohci
[ 0.223266] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for usbhs_ehci
[ 0.223266] omap_hwmod: l3_div_ck: missing clockdomain for l3_div_ck.
[ 0.225677] _omap4_module_wait_ready: Timeout waiting for module enable (mcpdm_fck: clkctrl = 0x30002)
[ 0.231445] omap_hwmod: mcpdm: cannot be enabled (3)
[ 0.233367] print_constraints: dummy:
[ 0.233367] NET: Registered protocol family 16
[ 0.233367] GPMC revision 6.0
[ 0.234924] EMIF0 is enabled with IRQ142
[ 0.234924] EMIF1 is enabled with IRQ143
[ 0.235015] Last reset was cold reset (PRM_RSTST=0x1)
[ 0.235015]
[ 0.235351] OMAP GPIO hardware version 0.1
[ 0.236145] omap_mux_init: Add partition: #1: core, flags: 2
[ 0.236602] omap_mux_init: Add partition: #2: wkup, flags: 2
[ 0.236602] omap_mux_get_by_name: Could not find signal uart1_cts.uart1_cts
[ 0.238281] omap_hwmod_mux_init: Could not allocate device mux entry
[ 0.243804] HSI: skipping omap_device registration
[ 0.243896] OMAP DMA hardware revision 0.0
[ 0.243896] omap_rproc_get_pool: dsp - no carveout memory is available at all
[ 0.244689] omap_rproc_get_pool: ipu - carveout memory is unavailable: 0x0, 0x0
[ 0.250427] bio: create slab <bio-0> at 0
[ 0.250732] print_constraints: vwl1271: 1800 mV
[ 0.251281] i2c-core: driver [twl] using legacy suspend method
[ 0.251281] i2c-core: driver [twl] using legacy resume method
[ 0.251281] SCSI subsystem initialized
[ 0.251739] usbcore: registered new interface driver usbfs
[ 0.251861] usbcore: registered new interface driver hub
[ 0.251953] usbcore: registered new device driver usb
[ 0.252563] omap_i2c omap_i2c.1: bus 1 rev4.0 at 400 kHz
[ 0.252563] Skipping twl internal clock init and using bootloader value (unknown osc rate)
[ 0.253662] twl6030: PIH (irq 39) chaining IRQs 368..387
[ 0.255584] print_constraints: VUSB: 3300 mV normal standby
[ 0.558654] twl6030_usb twl6030_usb: Initialized TWL6030 USB module
[ 0.559051] print_constraints: VMMC: 1200 <--> 3000 mV at 3000 mV normal standby
[ 0.559814] print_constraints: VPP: 1800 <--> 2500 mV at 1900 mV normal standby
[ 0.560485] print_constraints: VUSIM: 1200 <--> 2900 mV at 1800 mV normal standby
[ 0.561492] print_constraints: VCXIO: 1800 mV normal standby
[ 0.562469] print_constraints: VDAC: 1800 mV normal standby
[ 0.562774] print_constraints: VAUX1_6030: 1000 <--> 3000 mV at 1800 mV normal standby
[ 0.563140] print_constraints: VAUX2_6030: 1200 <--> 2800 mV at 1800 mV normal standby
[ 0.563781] print_constraints: VAUX3_6030: 1000 <--> 3000 mV at 1200 mV normal standby
[ 0.565002] print_constraints: VDD1:
[ 0.566162] print_constraints: VDD2:
[ 0.567169] print_constraints: V2V1: at 2100 mV
[ 0.568176] print_constraints: VANA: 2100 mV normal standby
[ 0.568908] print_constraints: CLK32KG:
[ 0.569641] print_constraints: CLK32KAUDIO:
[ 0.570617] print_constraints: SYSEN:
[ 0.571594] print_constraints: REGEN1:
[ 0.571716] omap_i2c omap_i2c.2: bus 2 rev4.0 at 400 kHz
[ 0.571929] omap_i2c omap_i2c.3: bus 3 rev4.0 at 100 kHz
[ 0.572235] omap_i2c omap_i2c.4: bus 4 rev4.0 at 400 kHz
[ 0.572235] omap-rproc omap-rproc.0: dsp is available
[ 0.572235] omap-rproc omap-rproc.1: ipu is available
[ 0.572235] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.572235] Bluetooth: Core ver 2.16
[ 0.573455] NET: Registered protocol family 31
[ 0.573455] Bluetooth: HCI device and connection manager initialized
[ 0.573455] Bluetooth: HCI socket layer initialized
[ 0.573486] Bluetooth: L2CAP socket layer initialized
[ 0.573486] Bluetooth: SCO socket layer initialized
[ 0.573547] Switching to clocksource 32k_counter
[ 0.575408] musb-hdrc: version 6.0, musb-dma, otg (peripheral+host)
[ 0.575592] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[ 0.575653] musb-hdrc: MHDRC RTL version 2.0
[ 0.575653] musb-hdrc: setup fifo_mode 4
[ 0.575653] musb-hdrc: 28/31 max ep, 16384/16384 memory
[ 0.575683] musb-hdrc musb-hdrc: USB Peripheral mode controller at fc0ab000 using DMA, IRQ 124
[ 0.576110] NET: Registered protocol family 2
[ 0.576110] IP route cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.576110] TCP established hash table entries: 131072 (order: 8, 1048576 bytes)
[ 0.576110] TCP bind hash table entries: 65536 (order: 8, 1572864 bytes)
[ 0.579864] Switched to NOHz mode on CPU #0
[ 0.579895] Switched to NOHz mode on CPU #1
[ 0.579925] TCP: Hash tables configured (established 131072 bind 65536)
[ 0.584045] TCP reno registered
[ 0.584045] UDP hash table entries: 512 (order: 3, 32768 bytes)
[ 0.584197] UDP-Lite hash table entries: 512 (order: 3, 32768 bytes)
[ 0.584197] NET: Registered protocol family 1
[ 0.585174] RPC: Registered named UNIX socket transport module.
[ 0.585174] RPC: Registered udp transport module.
[ 0.585174] RPC: Registered tcp transport module.
[ 0.585205] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.659942] omap_init_opp_table: no hwmod or odev for hsi, [18] cannot add OPPs.
[ 0.659973] omap_init_opp_table: no hwmod or odev for hsi, [19] cannot add OPPs.
[ 0.659973] ram_console: got buffer at a0000000, size 200000
[ 0.659973] ram_console: found existing buffer, size 40393, start 40393
[ 0.798919] console [ram-1] enabled
[ 0.798919] omap-iommu omap-iommu.0: ducati registered
[ 0.798919] omap-iommu omap-iommu.1: tesla registered
[ 0.832092] ashmem: initialized
[ 0.838287] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.838287] fuse init (API version 7.16)
[ 0.839324] msgmni has been set to 1295
[ 0.840942] io scheduler noop registered
[ 0.840942] io scheduler deadline registered
[ 0.841217] io scheduler cfq registered (default)
[ 0.841308] start plist test
[ 0.846008] end plist test
[ 0.846679] OMAP DSS rev 4.0
[ 0.848358] dsscomp: initializing.
[ 0.848358] misc dsscomp: display0=generic_dpi_panel
[ 0.848358] misc dsscomp: display1=hdmi_panel
[ 0.848907] misc dsscomp: found 2 displays and 4 overlays, WB overlay 1
[ 0.849243] could not allocate slot
[ 0.849639] omap-rproc omap-rproc.1: powering up ipu
[ 0.850036] virtio_rpmsg_bus virtio0: rpmsg backend virtproc probed successfully
[ 0.850036] virtio_rpmsg_bus virtio1: rpmsg backend virtproc probed successfully
[ 0.850036] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 104) is a OMAP UART0
[ 0.851928] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 105) is a OMAP UART1
[ 0.852386] omap_uart.2: ttyO2 at MMIO 0x48020000 (irq = 106) is a OMAP UART2
[ 1.977264] console [ttyO2] enabled
[ 1.981384] omap_uart.3: ttyO3 at MMIO 0x4806e000 (irq = 102) is a OMAP UART3
[ 1.989868] omap_ion_probe: adding heap secure_input of type 2 with ba300000@5a00000
[ 1.998687] omap_ion_probe: adding heap tiler of type 4 with ada00000@6000000
[ 2.006774] omap_ion_probe: adding heap nonsecure_tiler of type 4 with a0200000@2000000
[ 2.020202] brd: module loaded
[ 2.024658] loop: module loaded
[ 2.031280] (stk) :sysfs entries created
[ 2.035736] (stk) : debugfs entries created
[ 2.042633] PPP generic driver version 2.4.2
[ 2.042633] PPP Deflate Compression module registered
[ 2.054748] PPP BSD Compression module registered
[ 2.060668] PPP MPPE Compression module registered
[ 2.060760] NET: Registered protocol family 24
[ 2.060760] usbcore: registered new interface driver asix
[ 2.078643] usbcore: registered new interface driver cdc_ether
[ 2.085266] usbcore: registered new interface driver smsc95xx
[ 2.091827] usbcore: registered new interface driver net1080
[ 2.093475] usbcore: registered new interface driver cdc_subset
[ 2.104919] usbcore: registered new interface driver zaurus
[ 2.111175] cdc_ncm: 04-Aug-2011
[ 2.112854] usbcore: registered new interface driver cdc_ncm
[ 2.114898] usbcore: registered new interface driver zd1201
[ 2.126342] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.135070] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
[ 2.141326] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
[ 2.149658] ehci-omap ehci-omap.0: irq 109, io mem 0x4a064c00
[ 2.177459] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
[ 2.177459] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 2.177459] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.199493] usb usb1: Product: OMAP-EHCI Host Controller
[ 2.199493] usb usb1: Manufacturer: Linux 3.0.21-00003-OMAP-Android+ ehci_hcd
[ 2.213287] usb usb1: SerialNumber: ehci-omap.0
[ 2.218383] hub 1-0:1.0: USB hub found
[ 2.223052] hub 1-0:1.0: 3 ports detected
[ 2.254730] usbcore: registered new interface driver cdc_acm
[ 2.261047] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 2.269927] Initializing USB Mass Storage driver...
[ 2.275451] usbcore: registered new interface driver usb-storage
[ 2.275451] USB Mass Storage support registered.
[ 2.287261] usbcore: registered new interface driver usbserial
[ 2.287414] usbserial: USB Serial Driver core
[ 2.287414] USB Serial support registered for Keyspan - (without firmware)
[ 2.306427] USB Serial support registered for Keyspan 1 port adapter
[ 2.313537] USB Serial support registered for Keyspan 2 port adapter
[ 2.320617] USB Serial support registered for Keyspan 4 port adapter
[ 2.327758] usbcore: registered new interface driver keyspan
[ 2.334136] keyspan: v1.1.5:Keyspan USB to Serial Converter Driver
[ 2.558990] usb 1-1: new high speed USB device number 2 using ehci-omap
[ 2.642913] android_usb gadget: Mass Storage Function, version: 2009/09/11
[ 2.650512] android_usb gadget: Number of LUNs=1
[ 2.655700] lun0: LUN: removable file: (no medium)
[ 2.661346] android_usb gadget: android_usb ready
[ 2.666687] mousedev: PS/2 mouse device common for all mice
[ 2.676330] using rtc device, twl_rtc, for alarms
[ 2.676330] twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0
[ 2.688995] i2c /dev entries driver
[ 2.692871] lirc_dev: IR Remote Control driver registered, major 249
[ 2.700683] IR NEC protocol handler initialized
[ 2.700683] IR RC5(x) protocol handler initialized
[ 2.711029] IR RC6 protocol handler initialized
[ 2.714385] IR JVC protocol handler initialized
[ 2.721038] IR Sony protocol handler initialized
[ 2.726135] IR RC5 (streamzap) protocol handler initialized
[ 2.726135] IR LIRC bridge handler initialized
[ 2.737182] dmm: probe base: fd300000, irq 145
[ 2.742553] usb 1-1: New USB device found, idVendor=0424, idProduct=9514
[ 2.744415] OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
[ 2.745422] device-mapper: uevent: version 1.0.3
[ 2.746154] device-mapper: ioctl: 4.20.0-ioctl (2011-02-02) initialised: dm-devel@redhat.com
[ 2.746215] Bluetooth: HCI UART driver ver 2.2
[ 2.746215] Bluetooth: HCI H4 protocol initialized
[ 2.746246] Bluetooth: HCILL protocol initialized
[ 2.746246] Bluetooth: Bluetooth Driver for TI WiLink - Version 1.0
[ 2.792907] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 2.793914] cpuidle: using governor ladder
[ 2.793914] cpuidle: using governor menu
[ 2.794433] (stc): st_register(2)
[ 2.794433] (stc): chnl_id list empty :2
[ 2.794433] (stk) : st_kim_start
[ 2.803375] usbcore: registered new interface driver usbhid
[ 2.803375] usbhid: USB HID core driver
[ 2.832214] logger: created 256K log 'log_main'
[ 2.837371] logger: created 256K log 'log_events'
[ 2.842681] hub 1-1:1.0: USB hub found
[ 2.846984] logger: created 256K log 'log_radio'
[ 2.852081] hub 1-1:1.0: 5 ports detected
[ 2.856597] logger: created 256K log 'log_system'
[ 2.863037] OMAP HSI: HSI driver version 0.4.3
[ 2.868103] OMAP HSI: Platform DRIVER register FAILED: -19
[ 2.871582] ------------[ cut here ]------------
[ 2.871612] WARNING: at arch/arm/mach-omap2/omap_l3_noc.c:135 l3_interrupt_handler+0x2e0/0x380()
[ 2.871643] CUSTOM SRESP error with SOURCE:L4 PER2
[ 2.871643] Modules linked in:
[ 2.871643] Backtrace:
[ 2.871704] [<c00571b8>] (dump_backtrace+0x0/0x110) from [<c05e1e3c>] (dump_stack+0x18/0x1c)
[ 2.871704] r6:00000087 r5:c007aad0 r4:eb58da08 r3:eb58c000
[ 2.871734] [<c05e1e24>] (dump_stack+0x0/0x1c) from [<c009e140>] (warn_slowpath_common+0x5c/0x6c)
[ 2.871734] [<c009e0e4>] (warn_slowpath_common+0x0/0x6c) from [<c009e1f4>] (warn_slowpath_fmt+0x38/0x40)
[ 2.871734] r8:00000002 r7:f0834b48 r6:00080003 r5:c07db0fc r4:f0834b00
[ 2.871765] r3:00000009
[ 2.871765] [<c009e1bc>] (warn_slowpath_fmt+0x0/0x40) from [<c007aad0>] (l3_interrupt_handler+0x2e0/0x380)
[ 2.871765] r3:c071fae0 r2:c071f9e4
[ 2.871826] [<c007a7f0>] (l3_interrupt_handler+0x0/0x380) from [<c00e5d9c>] (handle_irq_event_percpu+0x58/0x188)
[ 2.871826] [<c00e5d44>] (handle_irq_event_percpu+0x0/0x188) from [<c00e5f10>] (handle_irq_event+0x44/0x64)
[ 2.871856] [<c00e5ecc>] (handle_irq_event+0x0/0x64) from [<c00e871c>] (handle_fasteoi_irq+0xa4/0x10c)
[ 2.871856] r6:0000002a r5:c07adb8c r4:c07adb40 r3:c004a4f0
[ 2.871887] [<c00e8678>] (handle_fasteoi_irq+0x0/0x10c) from [<c00e58c0>] (generic_handle_irq+0x40/0x48)
[ 2.871887] r5:c004ae80 r4:c07bc568
[ 2.871917] [<c00e5880>] (generic_handle_irq+0x0/0x48) from [<c004c060>] (asm_do_IRQ+0x60/0xc0)
[ 2.871948] [<c004c000>] (asm_do_IRQ+0x0/0xc0) from [<c00529c8>] (__irq_svc+0x48/0xe0)
[ 2.871948] Exception stack(0xeb58daf8 to 0xeb58db40)
[ 2.871948] dae0: eb58db28 00000000
[ 2.871978] db00: eb58c000 c07da1bc a0000113 c07d6f94 a0000113 c07dea04 3b9aca00 eb58dba0
[ 2.871978] db20: 00000000 eb58db54 ffffffff eb58db40 c05e56f4 c05e56f8 60000113 ffffffff
[ 2.871978] r7:00000002 r6:0000002a r5:fa240100 r4:ffffffff
[ 2.872009] [<c05e56e0>] (_raw_spin_unlock_irqrestore+0x0/0x44) from [<c00674bc>] (omap_hwmod_idle+0x3c/0x44)
[ 2.872039] r4:c07d6f48 r3:c07da1bc
[ 2.872070] [<c0067480>] (omap_hwmod_idle+0x0/0x44) from [<c0081e40>] (omap_device_idle_hwmods+0x30/0x44)
[ 2.872070] r6:00000000 r5:eb489e00 r4:00000001 r3:00000001
[ 2.872070] [<c0081e10>] (omap_device_idle_hwmods+0x0/0x44) from [<c0081f6c>] (_omap_device_deactivate+0x7c/0x118)
[ 2.872100] r5:c07dea04 r4:eb489e00
[ 2.872100] [<c0081ef0>] (_omap_device_deactivate+0x0/0x118) from [<c00821b4>] (omap_device_idle+0x28/0x74)
[ 2.872131] [<c008218c>] (omap_device_idle+0x0/0x74) from [<c00823c4>] (_od_runtime_suspend+0x24/0x2c)
[ 2.872131] r4:00000000
[ 2.872161] [<c00823a0>] (_od_runtime_suspend+0x0/0x2c) from [<c02f5a9c>] (rpm_callback+0x54/0x68)
[ 2.872161] r5:eb489e08 r4:c00823a0
[ 2.872192] [<c02f5a48>] (rpm_callback+0x0/0x68) from [<c02f5e28>] (rpm_suspend+0x110/0x494)
[ 2.872192] r6:00000000 r5:00000000 r4:eb489e08 r3:c07de290
[ 2.872222] [<c02f5d18>] (rpm_suspend+0x0/0x494) from [<c02f7138>] (__pm_runtime_suspend+0x80/0xac)
[ 2.872222] [<c02f70b8>] (__pm_runtime_suspend+0x0/0xac) from [<c02f3460>] (pm_generic_runtime_idle+0x4c/0x54)
[ 2.872222] r7:eb489e7c r6:c0082368 r5:eb489e08 r4:eb489e08
[ 2.872253] [<c02f3414>] (pm_generic_runtime_idle+0x0/0x54) from [<c0082378>] (_od_runtime_idle+0x10/0x14)
[ 2.872253] r4:00000000 r3:00000000
[ 2.872253] [<c0082368>] (_od_runtime_idle+0x0/0x14) from [<c02f6300>] (rpm_idle+0xe0/0x180)
[ 2.872283] [<c02f6220>] (rpm_idle+0x0/0x180) from [<c02f6488>] (__pm_runtime_idle+0x6c/0x98)
[ 2.872283] r7:60000113 r6:eb489e7c r5:00000004 r4:eb489e08
[ 2.872314] [<c02f641c>] (__pm_runtime_idle+0x0/0x98) from [<c03ab210>] (omap_i2c_idle+0x88/0xcc)
[ 2.872314] r7:c0853000 r6:eb4e4800 r5:eb489e08 r4:eb4e4800
[ 2.872344] [<c03ab188>] (omap_i2c_idle+0x0/0xcc) from [<c03ab620>] (omap_i2c_xfer+0x154/0x6b4)
[ 2.872344] r5:00000001 r4:eb4e48a8
[ 2.872375] [<c03ab4cc>] (omap_i2c_xfer+0x0/0x6b4) from [<c03a8118>] (i2c_transfer+0xb8/0xec)
[ 2.872406] [<c03a8060>] (i2c_transfer+0x0/0xec) from [<c03067b4>] (twl_i2c_write+0xb0/0x140)
[ 2.872406] [<c0306704>] (twl_i2c_write+0x0/0x140) from [<c030686c>] (twl_i2c_write_u8+0x28/0x30)
[ 2.872436] [<c0306844>] (twl_i2c_write_u8+0x0/0x30) from [<c02d0b08>] (twl6030reg_enable+0x68/0xac)
[ 2.872467] [<c02d0aa0>] (twl6030reg_enable+0x0/0xac) from [<c02cd7f4>] (_regulator_enable+0x180/0x284)
[ 2.872467] r6:00000000 r5:00000000 r4:eb4e5000
[ 2.872467] [<c02cd674>] (_regulator_enable+0x0/0x284) from [<c02cd91c>] (regulator_enable+0x24/0x38)
[ 2.872467] r6:eadae940 r5:eb4e5000 r4:eb4e5054 r3:00000000
[ 2.872528] [<c02cd8f8>] (regulator_enable+0x0/0x38) from [<c03d2d20>] (mmc_regulator_set_ocr+0xe4/0x128)
[ 2.872528] r5:eb5f7400 r4:00000000
[ 2.872558] [<c03d2c3c>] (mmc_regulator_set_ocr+0x0/0x128) from [<c03e5444>] (omap_hsmmc_1_set_power+0x6c/0xa8)
[ 2.872558] r8:00000000 r7:eb4ab008 r6:00000012 r5:00000001 r4:eb5f7740
[ 2.872558] r3:00000012
[ 2.872589] [<c03e53d8>] (omap_hsmmc_1_set_power+0x0/0xa8) from [<c03e38dc>] (omap_hsmmc_set_ios+0x428/0x488)
[ 2.872589] [<c03e34b4>] (omap_hsmmc_set_ios+0x0/0x488) from [<c03d251c>] (mmc_power_up+0x84/0xbc)
[ 2.872619] [<c03d2498>] (mmc_power_up+0x0/0xbc) from [<c03d394c>] (mmc_rescan+0x248/0x434)
[ 2.872619] r5:00061a80 r4:eb5f7400
[ 2.872650] [<c03d3704>] (mmc_rescan+0x0/0x434) from [<c00b5374>] (process_one_work+0x114/0x410)
[ 2.872650] r6:eb4f9800 r5:c0838200 r4:eadd1cc0 r3:00000001
[ 2.872680] [<c00b5260>] (process_one_work+0x0/0x410) from [<c00b5a18>] (worker_thread+0x1a8/0x490)
[ 2.872711] [<c00b5870>] (worker_thread+0x0/0x490) from [<c00bc654>] (kthread+0x94/0x98)
[ 2.872711] [<c00bc5c0>] (kthread+0x0/0x98) from [<c00a2a54>] (do_exit+0x0/0x720)
[ 2.872741] r7:00000013 r6:c00a2a54 r5:c00bc5c0 r4:eb44fe94
[ 2.872772] ---[ end trace 842a59dce0ffd309 ]---
[ 2.872772] Master 0x0 MPU
[ 2.872772] L4 PER2 OPCODE 0x00000000
[ 2.903808] (stk) :ldisc_install = 1
[ 3.319274] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 3.331604] mmc0: new high speed SDHC card at address 0007
[ 3.332000] mmcblk0: mmc0:0007 SD04G 3.70 GiB
[ 3.334594] mmcblk0: p1 p2
[ 3.498382] usbcore: registered new interface driver snd-usb-audio
[ 3.507202] SDP4430 SoC init
[ 3.514892] twl6040-codec twl6040-codec: couldn't get VDDHF regulator -19
[ 3.560638] asoc: null-codec-dai <-> MultiMedia1 mapping ok
[ 3.567718] asoc: null-codec-dai <-> MultiMedia2 mapping ok
[ 3.575012] asoc: null-codec-dai <-> Voice mapping ok
[ 3.581451] asoc: null-codec-dai <-> Tones mapping ok
[ 3.588012] asoc: null-codec-dai <-> Vibra mapping ok
[ 3.594268] asoc: null-codec-dai <-> MODEM mapping ok
[ 3.600494] asoc: null-codec-dai <-> MultiMedia1 LP mapping ok
[ 3.608093] asoc: FM Digital <-> omap-mcbsp-dai.1 mapping ok
[ 3.615295] asoc: twl6040-dl1 <-> mcpdm-dl mapping ok
[ 3.617431] mmc1: card claims to support voltages below the defined range. These will be ignored.
[ 3.632171] asoc: dmic-hifi <-> omap-dmic-dai-0 mapping ok
[ 3.639678] twl6040-codec twl6040-codec: ASoC: Failed to create Aux/FM Stereo In debugfs file
[ 3.649749] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
[ 3.656524] asoc: twl6040-dl1 <-> mcpdm-dl1 mapping ok
[ 3.663391] mmc1: new SDIO card at address 0001
[ 3.668823] asoc: twl6040-ul <-> mcpdm-ul1 mapping ok
[ 3.674987] asoc: twl6040-dl2 <-> mcpdm-dl2 mapping ok
[ 3.681365] asoc: twl6040-vib <-> mcpdm-vib mapping ok
[ 3.687683] asoc: Bluetooth <-> omap-mcbsp-dai.0 mapping ok
[ 3.694549] asoc: Bluetooth <-> omap-mcbsp-dai.0 mapping ok
[ 3.701385] asoc: FM Digital <-> omap-mcbsp-dai.1 mapping ok
[ 3.708251] asoc: MODEM <-> omap-mcbsp-dai.1 mapping ok
[ 3.714630] usb 1-1.1: new high speed USB device number 3 using ehci-omap
[ 3.722381] asoc: dmic-hifi <-> omap-dmic-abe-dai-0 mapping ok
[ 3.729370] asoc: dmic-hifi <-> omap-dmic-abe-dai-1 mapping ok
[ 3.736389] asoc: dmic-hifi <-> omap-dmic-abe-dai-2 mapping ok
[ 3.743408] asoc: null-codec-dai <-> omap-abe-vxrec-dai mapping ok
[ 3.752410] input: Panda Headset Jack as /devices/platform/soc-audio/sound/card0/input0
[ 3.763916] asoc: hdmi-audio-codec <-> hdmi-audio-dai mapping ok
[ 3.770996] ALSA device list:
[ 3.774291] #0: TI OMAP4 Board
[ 3.777862] #1: OMAP4HDMI
[ 3.781158] GACT probability NOT on
[ 3.785003] Mirror/redirect action on
[ 3.789031] u32 classifier
[ 3.792083] Actions configured
[ 3.795837] Netfilter messages via NETLINK v0.30.
[ 3.801055] nf_conntrack version 0.5.0 (10364 buckets, 41456 max)
[ 3.808868] ctnetlink v0.93: registering with nfnetlink.
[ 3.814727] NF_TPROXY: Transparent proxy support initialized, version 4.1.0
[ 3.822387] NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
[ 3.828948] xt_time: kernel timezone is -0000
[ 3.835510] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 3.841674] arp_tables: (C) 2002 David S. Miller
[ 3.846832] usb 1-1.1: New USB device found, idVendor=0424, idProduct=ec00
[ 3.854400] TCP cubic registered
[ 3.858673] NET: Registered protocol family 10
[ 3.863555] usb 1-1.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 3.876098] Mobile IPv6
[ 3.879211] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 3.885375] smsc95xx v1.0.4
[ 3.889038] IPv6 over IPv4 tunneling driver
[ 3.899047] NET: Registered protocol family 17
[ 3.904022] NET: Registered protocol family 15
[ 3.909271] Bridge firewalling registered
[ 3.913848] Bluetooth: RFCOMM TTY layer initialized
[ 3.919189] Bluetooth: RFCOMM socket layer initialized
[ 3.924865] Bluetooth: RFCOMM ver 1.11
[ 3.929016] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 3.934936] Bluetooth: BNEP filters: protocol multicast
[ 3.940673] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 3.947387] NET: Registered protocol family 35
[ 3.952545] lib80211: common routines for IEEE802.11 drivers
[ 3.958831] lib80211_crypt: registered algorithm 'NULL'
[ 3.964721] NET: Registered protocol family 37
[ 3.969635] Registering the dns_resolver key type
[ 3.974945] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 1
[ 3.983489] ThumbEE CPU extension supported.
[ 3.988281] Registering SWP/SWPB emulation handler
[ 3.998657] Reprogramming LPDDR2 timings to 400000000 Hz
[ 4.004791] sr_init: No PMIC hook to init smartreflex
[ 4.010498] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver initialized
[ 4.019226] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver initialized
[ 4.027954] smartreflex smartreflex.2: omap_sr_probe: SmartReflex driver initialized
[ 4.037170] Power Management for TI OMAP4.
[ 4.041931] OMAP4 PM: Static dependency added between MPUSS <-> EMIF, MPUSS <-> L4_PER/CFG MPUSS <-> L3_MAIN_1.
[ 4.052703] OMAP4 PM: Static dependency added between DUCATI <-> L4_PER/CFG and DUCATI <-> L3.
[ 4.061889] (stk) :ldisc installation timeout
[ 4.066467] (stk) :ldisc_install = 0
[ 4.075500] smsc95xx 1-1.1:1.0: eth0: register 'smsc95xx' at usb-ehci-omap.0-1.1, smsc95xx USB 2.0 Ethernet, 3a:34:c6:77:2b:42
[ 4.091979] clock: disabling unused clocks to save power
[ 4.183380] usb 1-1.2: new low speed USB device number 4 using ehci-omap
[ 4.312377] usb 1-1.2: New USB device found, idVendor=046d, idProduct=c05a
[ 4.319732] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 4.327514] usb 1-1.2: Product: USB Optical Mouse
[ 4.332611] usb 1-1.2: Manufacturer: Logitech
[ 4.340240] input: Logitech USB Optical Mouse as /devices/platform/omap/usbhs_omap/ehci-omap.0/usb1/1-1/1-1.2/1-1.2:1.0/input/input1
[ 4.353149] generic-usb 0003:046D:C05A.0001: input: USB HID v1.11 Mouse [Logitech USB Optical Mouse] on usb-ehci-omap.0-1.2/input0
[ 4.495178] cannot apply mgr(lcd) on inactive device
[ 4.501129] omapfb omapfb: failed to apply dispc config
[ 4.507141] cannot apply mgr(tv) on inactive device
[ 4.512969] omapfb omapfb: failed to apply dispc config
[ 4.518585] cannot apply mgr(lcd2) on inactive device
[ 4.524200] omapfb omapfb: failed to apply dispc config
[ 4.529907] omapdss DPI: Could not find exact pixel clock. Requested 74250 kHz, got 76800 kHz
[ 4.543151] regulator_init_complete: VUSB: incomplete constraints, leaving on
[ 4.551574] twl_rtc twl_rtc: setting system clock to 2000-01-01 00:09:25 UTC (946685365)
[ 4.561126] Waiting 2sec before mounting root device...
[ 5.253509] (stk) : timed out waiting for ldisc to be un-installed
[ 5.365844] (stk) :ldisc_install = 1
[ 6.519134] (stk) :ldisc installation timeout
[ 6.524444] (stk) :ldisc_install = 0
[ 6.582122] EXT2-fs (mmcblk0p2): warning: mounting ext3 filesystem as ext2
[ 6.590454] EXT2-fs (mmcblk0p2): warning: mounting unchecked fs, running e2fsck is recommended
[ 6.951934] VFS: Mounted root (ext2 filesystem) on device 179:2.
[ 6.963439] devtmpfs: mounted
[ 6.967163] Freeing init memory: 272K
[ 7.004913] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
[ 7.625335] omap-rproc omap-rproc.1: Loaded BIOS image ducati-m3.bin, size 6663880
[ 7.634887] omap-rproc omap-rproc.1: BIOS image version is 2
[ 7.641326] rproc_check_poolmem: section size does not fit within carveout memory
[ 7.649932] omap-rproc omap-rproc.1: static memory for IPU_MEM_IPC_VRING doesn't belong to poolmem
[ 7.660766] omap-rproc omap-rproc.1: Failed to process the image: -28
[ 7.683135] (stk) : timed out waiting for ldisc to be un-installed
[ 7.795745] (stk) :ldisc_install = 1
[ 8.948822] (stk) :ldisc installation timeout
[ 8.954101] (stk) :ldisc_install = 0
[ 10.112884] (stk) : timed out waiting for ldisc to be un-installed
[ 10.225006] (stk) :ldisc_install = 1
[ 11.378509] (stk) :ldisc installation timeout
[ 11.383605] (stk) :ldisc_install = 0
[ 12.542572] (stk) : timed out waiting for ldisc to be un-installed
[ 12.654754] (stk) :ldisc_install = 1
[ 13.808502] (stk) :ldisc installation timeout
[ 13.813781] (stk) :ldisc_install = 0
[ 14.972229] (stk) : timed out waiting for ldisc to be un-installed
[ 15.084503] (stk) :ldisc_install = 1
[ 16.237884] (stk) :ldisc installation timeout
[ 16.242980] (stk) :ldisc_install = 0
[ 17.401947] (stk) : timed out waiting for ldisc to be un-installed
[ 17.409027] Bluetooth: st_register failed -22
[ 25.325225] init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
[ 25.485229] Compat-wireless backport release:
[ 25.490051] Backport based on wl12xx.git v3.1-rc6-14178-gfb320e3
[ 25.759979] PVR: PVRCore_Init
[ 25.763702] PVR: PVRSRVDriverProbe(pDevice=eb4ad800)
[ 25.769958] PVR: SGX register base: 0x56000000
[ 25.774719] PVR: SGX register size: 65535
[ 25.779174] PVR: SGX IRQ: 53
[ 25.782287] PVR: EnableSystemClocks: Enabling System Clocks
[ 25.788848] PVR: PVRCore_Init: major device 248
[ 25.834808] omaplfbOMAPLFBInit: Blitsville gc2d not present, blits disabled
[ 25.842285] omaplfb: OMAPLFBInitIonOmap: Device 0: Requesting 2 TILER 2D framebuffers
[ 25.894012] cfg80211: Calling CRDA to update world regulatory domain
[ 26.367279] cfg80211: World regulatory domain updated:
[ 26.372802] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
[ 26.381744] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[ 26.390258] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
[ 26.398803] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
[ 26.407562] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[ 26.417114] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[ 26.914764] PVR: Installing MISR with cookie bf03fde8
[ 26.920715] PVR: Installing device LISR SGX ISR on IRQ 53 with cookie eafd4600
[ 26.928894] PVR: OSUnMapPhysToLin: unmapping 65535 bytes from f0be0000
[ 26.936035] PVR: SysFinalise: Version string: SGX revision = 1.2.0
[ 27.338500] wl12xx: driver version: BETA_01202012_01-1407-gd5e6ee8-dirty
[ 27.349731] wl12xx: compilation time: Sat Aug 18 20:55:34 2012
[ 27.358001] android_usb: already disabled
[ 27.362731] adb_bind_config
root@android:/ # [ 27.939849] adb_open
[ 28.222595] misc dsscomp: [ea662800] ignoring set failure -22
[ 42.244934] warning: `zygote' uses 32-bit capabilities (legacy support in use)
[ 47.044738] request_suspend_state: wakeup (3->0) at 47041320802 (2000-01-01 00:10:07.982116700 UTC)
[ 48.103515] init: no such service 'hciattach'
[ 48.108459] (stc): st_register(2)
[ 48.112030] (stc): chnl_id list empty :2
[ 48.120666] (stk) : st_kim_start
[ 48.250091] (stk) :ldisc_install = 1
[ 48.305389] (stc): st_tty_open
[ 48.310546] (stk) :line discipline installed
[ 48.315490] (stk) :TIInit_7.2.31.bts
[ 48.879058] (stc): add_channel_to_table: id 2
[ 48.883972] (stc): st_register(3)
[ 48.887603] (stc): add_channel_to_table: id 3
[ 48.892242] (stc): st_register(4)
[ 48.895782] (stc): add_channel_to_table: id 4
[ 49.664337] (stc): remove_channel_from_table: id 2
[ 49.669464] (stc): remove_channel_from_table: id 3
[ 49.674591] (stc): remove_channel_from_table: id 4
[ 49.679748] (stc): all chnl_ids unregistered
[ 49.684387] (stk) :ldisc_install = 0
[ 49.688293] (stc): st_tty_close
[ 49.890045] smsc95xx 1-1.1:1.0: eth0: link up, 100Mbps, full-duplex, lpa 0x45E1
[ 58.659698] eth0: no IPv6 routers present
[ 103.443908] acc_open
[ 103.446380] acc_release
[ 166.836578] request_suspend_state: sleep (0->3) at 166833129518 (2000-01-01 00:12:07.773955934 UTC)
[ 166.847869] DSSCOMP: dsscomp_early_suspend
[ 166.867736] DSSCOMP: blanked screen
root@android:/ #
root@android:/ #
root@android:/ # [ 194.363952] hpd 1
[ 194.409820] in hpd work 1, state=0
[ 194.413696] omapdss HDMI: ENTER hdmi_display_enable
[ 194.420684] omapdss HDMI: Set c-state constraint for HDMI
[ 194.420684]
[ 194.477996] hpd 0
[ 194.503540] in hpd work 0, state=1
[ 194.511749] omapdss HDMI: Enter hdmi_display_disable
[ 194.524993] omapdss HDMI: Release c-state constraint for HDMI
[ 194.524993]
[ 194.533905] hdmi: clearing EDID info
[ 194.727508] hpd 1
[ 194.737854] hpd 0
[ 194.769165] in hpd work 0, state=0
[ 194.987487] hpd 1
[ 195.003997] hpd 0
[ 195.034790] in hpd work 0, state=0
[ 195.253479] hpd 1
[ 195.300384] in hpd work 1, state=0
[ 195.304779] omapdss HDMI: ENTER hdmi_display_enable
[ 195.310485] omapdss HDMI: Set c-state constraint for HDMI
[ 195.310485]
[ 195.378509] in hpd work 2, state=1
[ 196.036468] edid[000] = 00 ff ff ff ff ff ff 00 10 ac 2c a0 53 56 33 30
[ 196.044036] edid[010] = 0a 13 01 03 80 34 20 78 ea b3 25 ac 51 30 b4 26
[ 196.051422] edid[020] = 10 50 54 a5 4b 00 81 80 a9 40 71 4f 01 01 01 01
[ 196.058532] edid[030] = 01 01 01 01 01 01 28 3c 80 a0 70 b0 23 40 30 20
[ 196.065673] edid[040] = 36 00 07 44 21 00 00 1a 00 00 00 ff 00 47 32 39
[ 196.072753] edid[050] = 33 48 39 33 34 30 33 56 53 0a 00 00 00 fc 00 44
[ 196.079895] edid[060] = 45 4c 4c 20 32 34 30 38 57 46 50 0a 00 00 00 fd
[ 196.086944] edid[070] = 00 38 4c 1e 53 11 00 0a 20 20 20 20 20 20 01 1f
[ 196.094024] edid[080] = 02 03 1b f1 48 90 05 04 03 02 07 16 01 23 09 07
[ 196.101104] edid[090] = 07 65 03 0c 00 10 00 83 01 00 00 02 3a 80 18 71
[ 196.108123] edid[0a0] = 38 2d 40 58 2c 45 00 07 44 21 00 00 1e 01 1d 80
[ 196.115417] edid[0b0] = 18 71 1c 16 20 58 2c 25 00 07 44 21 00 00 9e 01
[ 196.122436] edid[0c0] = 1d 00 72 51 d0 1e 20 6e 28 55 00 07 44 21 00 00
[ 196.129516] edid[0d0] = 1e 8c 0a d0 8a 20 e0 2d 10 10 3e 96 00 07 44 21
[ 196.136566] edid[0e0] = 00 00 18 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.143615] edid[0f0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 47
[ 196.150726] edid[100] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.157989] edid[110] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.165069] edid[120] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.172119] edid[130] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.179199] edid[140] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.186279] edid[150] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.193298] edid[160] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.200378] edid[170] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.207427] edid[180] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.214508] edid[190] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.221588] edid[1a0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.229034] edid[1b0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.236145] edid[1c0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.243164] edid[1d0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.250244] edid[1e0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.257293] edid[1f0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 196.264434] panel size 52 by 32
[ 196.272186] omapdss HDMI: Enter omapdss_hdmi_display_set_mode
[ 196.280487] omapdss HDMI: Enter hdmi_display_disable
[ 196.293914] omapdss HDMI: Release c-state constraint for HDMI
[ 196.293914]
[ 196.301910] hdmi: clearing EDID info
[ 196.305755] omapdss HDMI: ENTER hdmi_display_enable
[ 196.311187] omapdss HDMI: Set c-state constraint for HDMI
[ 196.311187]
[ 196.417572] omapdss DISPC error: timeout waiting for EVSYNC
root@android:/ #
root@android:/ #
root@android:/ #
========================================================================