Hi,
I would like to have some comment on performance of DM365 SDIO.
I created an SDIO driver for DM365 using SDIO patch contained in Kernel 2.6.18 REL_LSP_01_30_01_091.
(I referred to the info. on http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/t/7581.aspx#29891)
As I run Marvell WLAN driver using this driver, the wireless rate is only around 5Mbps at maximum.
The datasheet "LSP_1.30_Drivers_Data_Sheet_SPRS495.pdf" section "2.18 SDIO WLAN Driver",
"2.18.7 Performance and Benchmarks" reads;
"Infrastructure - 802.11g Up-Link:3.72 Downlink:3.91".
I'm wondering if this actually is reasonable value.
Please advise if the maximum 5Mbps we are having is reasonable and typical value for Marvell WLAN driver performance.
Thanks,
Katsumi