My problem is that my pandaboard es rev b1(omap4460) can't boot from linux minimal-fs.I have done the step according to http://omappedia.org/wiki/Minimal-FS. But the board didn't boot and there was no information printed form serial port. I suspected that was the mismatch problem. So I downloaded and compiled several different versions of source code of bootloader from linaro.org, gitorious.org,denx.de and so on. Unfortunately, These're failed too. However it can boot up from ubuntu 11.10. So what should I do if I want to boot linux minimal-fs from SD card?