Other Parts Discussed in Thread: 4460, 4430
Hi all,
Can anyone provide me C driver code for hmc5883l 3 axis compass for my custom omap 4460 platform (Android ICs)
Thanks
Abhijit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Abhijit,
Included with the TI OMAP4460 ICS releases are compass drivers for only AK8975 and HMC5843 (/kernel/android-3.0/drivers/staging/iio/magnetometer). You will need to adapt one of these drivers to meet your needs or check with the vendor of your compass if there is already a driver available.
Regards,
Gina
Hi Gina,
ICS release has two drivers one is kernel/android-3.0/drivers/staging/iio/magnetometer and the other one is kernel/android-3.0/drivers/input/misc/hmc5843.c.
Can you tell me which one to use.
Thanks
Abhijit
Abhijit,
It looks like the driver currently used for Blaze and Blaze Tablet is in kernel/android-3.0/drivers/input/misc/hmc5843.c. In /drivers/input/misc/Makefile:
obj-$(CONFIG_INPUT_HMC5843) += hmc5843.o
Compared to /drivers/staging/iio/magnetometer/Makefile:
obj-$(CONFIG_SENSORS_HMC5843) += hmc5843.o
In /arch/arm/mach-omap2/Kconfig:
config MACH_OMAP_4430SDP
bool "OMAP 4430 SDP board"
default y
depends on ARCH_OMAP4
select LEDS_OMAP4430_SDP_DISPLAY
select LEDS_OMAP4430_SDP_KEYPAD
select SENSORS_LM75
select INPUT_BH1780
select INPUT_BMP085
select INPUT_HMC5843
....
You will want to check if this is the same in the setup you are using.
Regards,
Gina
Abhijit,
Please see post http://e2e.ti.com/support/omap/f/849/t/212814.aspx for some information about a driver for HMC5883.
Regards,
Gina