Hi,TI guys:
I am working on PA_multicore Example trying to change it to suit my own application while I encounter a Length problem. There are two relevant registers, Mac Receive mac lenth registers and Port 0 receive lenth Register. Both are configured to 1518. But in the Gbe switch doc, the max lentgh of Mac is 16383, while the Port 0 max receive length is 9504. Since the packet will go through both module from Ethernet to Dsp, why is the value not the same? And what's the maximum receive length of the whole network coproccesser? How shall I set the regiser then?
Looking forward to your answer!
Best regards,
David