Other Parts Discussed in Thread: DM3730
Hi,
We are trying to change the fps to 15. But Capture parameter setformat is failing. It is allowing only 25 or 30.
Following are the details
platform - EVM DM3730
OS - wince 6.0
Application - CaptureTest
cmd :: CaptureTest /auto /pv /cap 352x288@15 /venc h264
Can we know the procedure to change fps ? Do we need to change the camera driver??
Is h264 supports FPS the other than 25 and 30?
Thanks,