Other Parts Discussed in Thread: OMAP-L138
Hi there,
I have searched through many threads and wikis for the solution to my problem and I think that this thread is the most relevant place for me to comment on, so my apologies if I have missed the information I was looking for.
I recently purchased a C6748 LCDK for use with my honours thesis. I got the demonstration programs operating quickly, confirming that the serial port is configured correctly.
My application required me to pass audio from the audio input to output and I found an audio example intended for the C6748 EVM that seemed to be a very useful template.
I am using CCSv5 and set up the target configuration using the LCDK gel supplied on the wiki.
When I try to connect I get the following error:
ICEPICK_C: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located. (Emulation package 5.0.747.0)
I noted in other threads that there is no onboard emulation for the LCDK. Can you please confirm this?
Are you able to direct me to any other examples that might suit my requirements?
I would appreciate any advice you can provide.
Regards,
Ed.