This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HPI Boot issue for C6482



We have been having an issue with the HPI boot process.  It seems to come and go and be highly dependent on the particular build.  I have found a similar problem from another post listed below:

http://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/p/153708/567375.aspx#567375

In this post one of the comments has this claim:

But then again, running in a bad code space can cause similar symptoms. All of the C6713's peripherals (HPI, JTAG, EDMA, etc) have memory mapped registers, many of them "Reserved", and rogue code that overwrites the registers repeatedly can lock up the peripheral requiring a hard reset.

When we have talked to TI about this issue previously, a POR reset was thought to be able to get any "crashed" code out of this state.  The above statement seems to suggest otherwise.  I assume the hard reset is a power reset.

Can you confirm if the above statement is true for the C6482 and that some cases will require a power reset to clear some issues?

Regards,

Dan

  • Dan,

    There is no C6482 device, so I assume you mean TCI6482. TCI6xxx devices are not supported on the forum.  They are supported through your local Field Application Engineering team.  Please work with them. If you are not sure who your local Field Application Engineer is, please work with your local sales representative to find out who they are.

    POR = Power On Reset

    The TCI6482 is two generations newer than a C6713, so it probably has some improvements over the older part. I am not sure how I missed it, but I could not find that "claim" on the thread you listed above.

    Regards,
    RandyP