Hello,
We are using several OMAPL137 for our development , and we realized that with one of them we are unable to boot properly from u-boot.
After boot we get 'Warning - Bad CRC ...." , and when running "sf probe 0" we get "fail to initialize SPI flash"
We found that the difference is in the assembled SPI flash type (the working boards are using 25x32 , while the unworking has the 25q32 ) these flash are different in their winbond ID (0x3016 for the 'good' board and 0x4016 for the 'bad' board).
We assume this is related to the u-boot code programed in the flash
pls help us to resolve this issue ASAP / send us a proper u-boot code.
Tnx,
Gilad