Other Parts Discussed in Thread: AM3517
Hello, I have been trying to move my platform from 2.6.37 to 3.3.7 kernel but coming across some booting issues. It seems as though I cant get the frame buffer initialised and the on chip phy. The boot log is :
NAND read: device 0 offset 0x280000, size 0x400000
4194304 bytes read: OK
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-3.3.7
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2712288 Bytes = 2.6 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0
[ 0.000000] Linux version 3.3.7 (marcmltd@fedora15.marcmltd) (gcc version 4.5.2 (Sourcery G++ Lite 2011.03-41) ) #4 Sun Sep 9 22:10:42 BST 2012
[ 0.000000] CPU: ARMv7 Processor [411fc087] revision 7 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
[ 0.000000] Machine: TAM3517
[ 0.000000] Reserving 12582912 bytes SDRAM for VRAM
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM3517 ES1.1 (l2cache iva sgx neon isp )
[ 0.000000] Clocking rate (Crystal/Core/MPU): 26.0/332/500 MHz
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 61696
[ 0.000000] Kernel command line: console=ttyO0,115200n8 mem=256M mpurate=600 omapdss.def_disp=lcd omapfb.vram=0:4M,1:4M,2:4M vram=12M tnlcd.tnlcd_data=8000,480,8,4,41,272,4,2,10,24,32 omap_vout.vid1_static_vrfb_alloc=y root=/dev/nfs rw nfsroot=10.0.0.11:/home/marcmltd/ICU_Devel/buildroot_dev/buildroot-2012.05/output/target rootfstype=nfs ip=dhcp rw
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 243MB = 243MB total
[ 0.000000] Memory: 240764k/240764k available, 21380k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc04f8000 (5056 kB)
[ 0.000000] .init : 0xc04f8000 - 0xc0525000 ( 180 kB)
[ 0.000000] .data : 0xc0526000 - 0xc05700c0 ( 297 kB)
[ 0.000000] .bss : 0xc05700e4 - 0xc05a4904 ( 211 kB)
[ 0.000000] NR_IRQS:460
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts
[ 0.000000] Total of 96 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000274] Calibrating delay loop... 497.82 BogoMIPS (lpj=1941504)
[ 0.039093] pid_max: default: 32768 minimum: 301
[ 0.039337] Mount-cache hash table entries: 512
[ 0.039886] CPU: Testing write buffer coherency: ok
[ 0.040283] Setting up static identity map for 0x803c4ec0 - 0x803c4f18
[ 0.041168] devtmpfs: initialized
[ 0.043365] omap_hwmod: usbtll_fck: missing clockdomain for usbtll_fck.
[ 0.044799] omap_hwmod: am35x_otg_hs: cannot be enabled (3)
[ 0.046752] print_constraints: dummy:
[ 0.047241] NET: Registered protocol family 16
[ 0.047760] GPMC revision 5.0
[ 0.051727] gpiochip_add: registered GPIOs 0 to 31 on device: gpio
[ 0.051818] OMAP GPIO hardware version 2.5
[ 0.052185] gpiochip_add: registered GPIOs 32 to 63 on device: gpio
[ 0.052612] gpiochip_add: registered GPIOs 64 to 95 on device: gpio
[ 0.053039] gpiochip_add: registered GPIOs 96 to 127 on device: gpio
[ 0.053466] gpiochip_add: registered GPIOs 128 to 159 on device: gpio
[ 0.053894] gpiochip_add: registered GPIOs 160 to 191 on device: gpio
[ 0.056640] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.061065] Reprogramming SDRC clock to 332000000 Hz
[ 0.061096] dpll3_m2_clk rate change failed: -22
[ 0.062469] usbhs_omap: alias fck already exists
[ 0.064605] _omap_mux_init_gpio: Multiple gpio paths (2) for gpio126
[ 0.076171] omap-mcbsp.2: alias fck already exists
[ 0.076629] omap-mcbsp.3: alias fck already exists
[ 0.078643] Calibrating delay loop (skipped) already calibrated this CPU
[ 0.078796] Switched to new clocking rate (Crystal/Core/MPU): 26.0/332/600 MHz
[ 0.078979] OMAP DMA hardware revision 4.0
[ 0.110778] bio: create slab <bio-0> at 0
[ 0.113250] SCSI subsystem initialized
[ 0.116577] usbcore: registered new interface driver usbfs
[ 0.116882] usbcore: registered new interface driver hub
[ 0.117156] usbcore: registered new device driver usb
[ 0.118927] omap_i2c omap_i2c.1: bus 1 rev1.3.12 at 400 kHz
[ 0.120239] print_constraints: VDCDC1: 1200 <--> 1600 mV at 1200 mV normal
[ 0.120849] print_constraints: VDCDC2: 1800 mV normal
[ 0.121276] print_constraints: VDCDC3: 1800 <--> 3300 mV at 1800 mV normal
[ 0.121734] print_constraints: LDO1: 1800 mV normal
[ 0.122283] print_constraints: LDO2: 3300 mV normal
[ 0.132904] omap_i2c omap_i2c.2: bus 2 rev1.3.12 at 400 kHz
[ 0.148529] omap_i2c omap_i2c.3: bus 3 rev1.3.12 at 400 kHz
[ 0.150970] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.153045] cfg80211: Calling CRDA to update world regulatory domain
[ 0.153320] Switching to clocksource 32k_counter
[ 0.178771] usbhs_omap usbhs_omap: xclk60mhsp1_ck set parentfailed error:-22
[ 0.179992] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.180145] musb-hdrc musb-hdrc: musb_init_controller failed with status -19
[ 0.180816] NET: Registered protocol family 2
[ 0.181060] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.181549] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.181793] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.181945] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.181945] TCP reno registered
[ 0.181976] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.182006] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.182220] NET: Registered protocol family 1
[ 0.182708] RPC: Registered named UNIX socket transport module.
[ 0.182708] RPC: Registered udp transport module.
[ 0.182739] RPC: Registered tcp transport module.
[ 0.182739] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.182922] omap_init_opp_table: no hwmod or odev for iva, [8] cannot add OPPs.
[ 0.187164] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.187225] msgmni has been set to 470
[ 0.188262] io scheduler noop registered
[ 0.188323] io scheduler cfq registered (default)
[ 0.190002] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.192352] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 72) is a OMAP UART0
[ 0.801635] console [ttyO0] enabled
[ 0.805969] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 73) is a OMAP UART1
[ 0.813995] omap_uart.2: ttyO2 at MMIO 0x49020000 (irq = 74) is a OMAP UART2
[ 0.821960] omap_uart.3: ttyO3 at MMIO 0x4809e000 (irq = 84) is a OMAP UART3
[ 0.830902] [drm] Initialized drm 1.1.0 20060810
[ 0.837493] GPIO NAND driver, © 2004 Simtec Electronics
[ 0.843811] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xbc (Micron NAND 512MiB 1,8V 16-bit)
[ 0.853424] Creating 5 MTD partitions on "omap2-nand.0":
[ 0.859069] 0x000000000000-0x000000080000 : "X-Loader"
[ 0.866455] 0x000000080000-0x000000260000 : "U-Boot"
[ 0.874053] 0x000000260000-0x000000280000 : "U-Boot Env"
[ 0.881378] 0x000000280000-0x000000680000 : "Kernel"
[ 0.889678] 0x000000680000-0x000020000000 : "File System"
[ 1.073547] davinci_mdio davinci_mdio.0: failed to get device clock
[ 1.080291] davinci_mdio: probe of davinci_mdio.0 failed with error -2
[ 1.087707] usbcore: registered new interface driver cdc_ether
[ 1.094177] usbcore: registered new interface driver cdc_ncm
[ 1.100158] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.107177] _regulator_get: ehci-omap.0 supply hsusb0 not found, using dummy regulator
[ 2.122222] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
[ 2.128265] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
[ 2.136230] ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
[ 2.153533] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
[ 2.159667] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 2.166839] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.174438] usb usb1: Product: OMAP-EHCI Host Controller
[ 2.180023] usb usb1: Manufacturer: Linux 3.3.7 ehci_hcd
[ 2.185607] usb usb1: SerialNumber: ehci-omap.0
[ 2.191467] hub 1-0:1.0: USB hub found
[ 2.195526] hub 1-0:1.0: 3 ports detected
[ 2.224334] usbcore: registered new interface driver uas
[ 2.229888] Initializing USB Mass Storage driver...
[ 2.235382] usbcore: registered new interface driver usb-storage
[ 2.241699] USB Mass Storage support registered.
[ 2.246978] mousedev: PS/2 mouse device common for all mice
[ 2.254455] rtc-ds1307 3-0068: rtc core: registered ds1307 as rtc0
[ 2.261047] rtc-ds1307 3-0068: 56 bytes nvram
[ 2.265838] i2c /dev entries driver
[ 2.271240] lirc_dev: IR Remote Control driver registered, major 252
[ 2.278015] IR NEC protocol handler initialized
[ 2.282836] IR RC5(x) protocol handler initialized
[ 2.287872] IR RC6 protocol handler initialized
[ 2.292633] IR JVC protocol handler initialized
[ 2.297454] IR Sony protocol handler initialized
[ 2.302337] IR RC5 (streamzap) protocol handler initialized
[ 2.308166] IR SANYO protocol handler initialized
[ 2.313110] IR MCE Keyboard/mouse protocol handler initialized
[ 2.319244] IR LIRC bridge handler initialized
[ 2.323913] Linux video capture interface: v2.00
[ 2.330230] OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
[ 2.343658] usbcore: registered new interface driver usbhid
[ 2.349578] usbhid: USB HID core driver
[ 2.356933] ALSA device list:
[ 2.360046] No soundcards found.
[ 2.363891] TCP cubic registered
[ 2.367614] NET: Registered protocol family 17
[ 2.372344] NET: Registered protocol family 15
[ 2.377014] can: controller area network core (rev 20090105 abi 8)
[ 2.383636] NET: Registered protocol family 29
[ 2.388366] can: raw protocol (rev 20090105)
[ 2.392883] can: broadcast manager protocol (rev 20090105 t)
[ 2.401580] lib80211: common routines for IEEE802.11 drivers
[ 2.407592] Registering the dns_resolver key type
[ 2.412658] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1
[ 2.421325] voltdm_scale: No voltage scale API registered for vdd_mpu_iva
[ 2.428527] voltdm_scale: No voltage scale API registered for vdd_core
[ 2.435424] PM: no software I/O chain control; some wakeups may be lost
[ 2.442779] clock: disabling unused clocks to save power
[ 2.450958] omapfb omapfb: no displays
[ 2.454895] omapfb omapfb: failed to setup omapfb
[ 2.460052] omapfb: probe of omapfb failed with error -22
[ 2.466247] davinci_emac davinci_emac: failed to get EMAC clock
[ 2.472473] davinci_emac: probe of davinci_emac failed with error -16
Hopefully someone has already solved this issue to stop me pulling my hair out. If I could get the phy up I could then continue to boot NFS. At least thats the theory.
Thanks in advance
Marc