This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCIE throughput issue



Hi,

I have a DaVinci DM8168 EVM with our DM8168 board connected via PCIe.

In RC side we will allocate a buffer for data using kmalloc() and an ioremap() address point to EP buffer,

Then we measure the throughput as following,

using memcpy:

   EP  write to RC buffer around 50MB/s   

   EP  read from RC buffer only 5MB/s

using EDMA in EP side:

   EP write to RC buffer 23MB/s   

   EP read from RC buffer 22MB/s

Questions:

   1. The throughput is reasonable?   

   2. Our application is EP decode video stream, our design is right?  I means using the RAM buffer in RC instead of EP.

 

  Regards,

 

Vic.