Hi,
I have a couple of queries regarding the DDR2 routing recommendations in the AM335x datasheet (sprs717d).
* Section 5.5.2.2.2.9 specifies for the Data net classes "No external termination resistors are allowed and ODT must be used for these net classes". However, I noticed that all the dev boards (BeagleBone, AM335x EVM, etc) do use series termination resistors on these signals. It will make the board a lot easier to route if I do not need these resistors however we have a very tight development schedule and can not afford to do a redesign if there is an issue. Would you consider it safe to run without the termination resistors on the data nets?
* The example PCB stack-ups in the datasheet suggest that the DDR2 1.8V power plane can be used as a signal return plane however an app note by Analog Devices states that "Power planes cannot be used as signal return for the DDR2 interface" (Page 3 of http://www.analog.com/static/imported-files/application_notes/EE349_rev2.pdf). Is this correct?
Kind Regards
Mark