Hi all,
I'm using the TMS320DM8168 EVM board .
I just started the sys/bios programming.
I am referring the ti sys/bios video.
Now I am succeeded in running a small code on this board with sys bios.
I want to run the "LED BLINK "project on this board.
I made this project and when I run this, pointer hit the main function and then I press resume button ,i am not able to see any led is blinking and when i press suspend button i got below error:
Can't find a source file at "C:\sandboxsvn\Freon\SE\trunk\src\c6748\bsl\src/evmc6748_i2c.c"
Locate the file or edit the source lookup path to include its location.
If it will run also which led will blink ??
Weather ON/OFF status led will blink or some other led will blink on that board TMS320DM8168 EVM board ....
I am new to this.Please guide me.....
-Studinstru