This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power Required to implement H.264 using DM368

We are doing a  review on H.264.  We are looking into the DM368.  Could you help get an estimate of what the total power would be, DSP as well as peripheral device(s) such as required memory to run H.264?  We played with the excel spreadsheet and got a number of 720mW to 768mW, but I don’t believe it includes the memory device require to run the encoder.  Do you have any measured value from any test that TI completed?

 thanks