This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ducati for Jelly Bean board with 512M of RAM



Hi.

In the Jelly Bean kernel, the file arch/arm/mach-omap2/remoteproc.c specifies what ducati firmware module should be loaded.  It is based on the amount of RAM on the board.  For a 1G board, it specifies ducati-m3.bin.  For a 512M board, it specifies ducati-m3.512MB.bin.

The tarballs device/ti/proprietary-open/omap4/ducati_blaze_tablet.tgz and device/ti/proprietary-open/omap4/ducati_full_blaze.tgz only contain ducati-m3.bin.

Where can I find ducati-m3.512MB.bin?

Regards,

    Steve