This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VLIB Connected components labeling - memory error



Hi,

Im using the connected components labeling api implemented in the vision library. The Api VLIB_calcConnectedComponentsMaxBufferSize offers the number of bytes required. For a 352x225 image this api is returning the value 2419180(about 2 mb).  First of all, this value seems to be very large.The other problem is that even this value is not enough. When 2419180 bytes is allocated statically, the creation of a connected components list fails(Error: Memory Allocation Failure). When allocating 2xmaxbytes, the creation of a connected components list works. Is there a bug in the library???I hope i would get an answer to my question since im applying this interface in my thesis.

Thank you.

Best regards,

Omar