Other Parts Discussed in Thread: OMAP3530
Hello.
I use the BSP Version 2.30.00.01 with WEC7.
Now I have the problem, that the registry hive didn't work.
Have anyone a solution for the reg hive in NAND-Flash and booting from NAND-Flash?
When I use the original NAND.REG, I have the following result:
First boot: EBOOT format the flash, after starting the image I change a registry key (touch calibration)
Next boot: WEC7 format the flash and the registry setting is lost
Next boot: EBOOT format the flash and the image is lost.
Please, have anyone a solution or the same problem?
Best regards
Jürgen