Other Parts Discussed in Thread: DM3730
Hi,
2.6.37, EVM, DM3730
I want to wake up the system from idle by usb wakeup - at this moment I'm only interested in wakeup event.
How should it be done when usbhost domain is in ret and usb functional/interface clocks are cut off ?
In pm34xx.c I see that:
/* Enable wakeups in PER */
omap2_prm_write_mod_reg(omap3630_en_uart4_mask |
OMAP3430_EN_GPIO2_MASK | OMAP3430_EN_GPIO3_MASK |
OMAP3430_EN_GPIO4_MASK | OMAP3430_EN_GPIO5_MASK |
OMAP3430_EN_GPIO6_MASK | OMAP3430_EN_UART3_MASK |
OMAP3430_EN_MCBSP2_MASK | OMAP3430_EN_MCBSP3_MASK |
OMAP3430_EN_MCBSP4_MASK,
OMAP3430_PER_MOD, PM_WKEN);
/* and allow them to wake up MPU */
omap2_prm_write_mod_reg(omap3630_grpsel_uart4_mask |
OMAP3430_GRPSEL_GPIO2_MASK |
OMAP3430_GRPSEL_GPIO3_MASK |
OMAP3430_GRPSEL_GPIO4_MASK |
OMAP3430_GRPSEL_GPIO5_MASK |
OMAP3430_GRPSEL_GPIO6_MASK |
OMAP3430_GRPSEL_UART3_MASK |
OMAP3430_GRPSEL_MCBSP2_MASK |
OMAP3430_GRPSEL_MCBSP3_MASK |
OMAP3430_GRPSEL_MCBSP4_MASK,
OMAP3430_PER_MOD, OMAP3430_PM_MPUGRPSEL);
Which mask should be used for usbhost?
How usb phy generate wakeup event ?
Karol