Spruec6g, pg 14. describes the I2C EEPROM boot mode which allows a sequence of Boot Parameter and Boot Configuration tables to be provided to the bootloader.
We would like to use a similar sequence of Boot Parameter and Boot Configuration Tables but using the I2C slave boot mode. Is this possible?
In particular we would like an FPGA to act as a I2C master and supply the Boot Parameter and Configuration tables to the C6455 acting as an I2C slave. This is useful as an EEPROM is already on the C6455's I2C bus and this device cannot be used to hold boot data.