Hi,
I'm trying to make two C6678 EVM boards talk through SRIO. My question is: Can I directly connect the two without a SRIO switch?
If I do need a switch, where can I get a stard alone one? (My google search only shows SRIO switch chip)
I connect SRIO lane 0 of the two EVM boards with two "AMC SMA ULTRA 9000" boards (http://silicontkx.com/SMA-AMCULTRA9000.html) and SMC 4 cables, but couldn't make it work.
Thanks,
Weiyi