If use the latest u-boot (2012) on the same board which has DM355 processor, i see DRAM: 64 MiB and NAND: 256 MiB
when i use 2010 u-boot on the same board which has the same DM355 processor, i see DRAM: 128 MiB and NAND: 128 MiB, how can this be possible ?
*************** 2012 u-boot Release *********************
U-Boot 2012.07 (Sep 05 2012 - 15:37:40)
I2C: ready
DRAM: 64 MiB
NAND: 256 MiB
**************** 2010 u-boot Release *********************
U-Boot 2010.06 (Aug 17 2010 - 14:56:30)
Cores: ARM 216 MHz
DDR: 133 MHz
I2C: ready
DRAM: 128 MiB
NAND: 128 MiB