Other Parts Discussed in Thread: OMAP-L138
hi,
I am using the Logic PD Experimenter with OMAP-L138 SOM, i built my code on the example of the training workshop Sol3_THREADS. i modified the initialization of the MCASP to make clock source AUXCLK (24 MHz) by setting CLKXM=1 and HCLKXM=1. but it appears that is impossible if we used 16 or 32 slot size because 24000000/(8000*32)= 93.75 or 24000000/(8000*64)= 46.875 . i tried to change the slot size on the reg RFMT and XFMT to 20 because 24000000/(8000*40)=75 but i failed to get any output.
is there any solution to set the McASP to 8 KHz without replacing the external AHCLKX to smaller value such as 3.072?
here is my initialization of the McASP:
// configure transmit registers for I2S - all same as above
MCASP->XMASK = 0xFFFFF000;
MCASP->XFMT = 0x00018098;
MCASP->AFSXCTL = 0x00000112;
MCASP->ACLKXCTL = 0x000000A0;
MCASP->AHCLKXCTL = 0x0000804a;
MCASP->XTDM = 0x00000003;
MCASP->XINTCTL = 0x00000000;
MCASP->XCLKCHK = 0x00FF0008;
// config serializers (11 = xmit, 12 = rcv)
MCASP->SRCTL11 = 0x000D; // XMT
MCASP->SRCTL12 = 0x000E; // RCV
// config pin function and direction.
MCASP->PFUNC = 0;
MCASP->PDIR = 0x14000800;
MCASP->DITCTL = 0x00000000;
MCASP->DLBCTL = 0x00000000;
MCASP->AMUTE = 0x00000000;