Other Parts Discussed in Thread: AM3359
I have a project built, ready to be flased onto the ICE.
I am working with both a windows 7 and a windows xp machine. In both cases, when I attempt to connect to the device, I get this error:
**
This error is generated by TI's USCIF driver or utilities.
The value is '-151' (0xffffff69). The title is 'SC_ERR_FTDI_OPEN'.
The explanation is: One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located.
**
The target configuration is for a am3359 for the ICE,with the xds100 usb emulator
Any ideas what could be the issue here?
-colin