This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB FIFO Size Defines



C6748_StarterWare_1_20_03_03. Some doubt about the correctness of the USB FIFO defines in usb.h. The existing code:

#define USB_FIFO_SZ_8192        0x00000010 // Biju

#define USB_FIFO_SZ_8_DB        0x00000011  // 8 byte double buffered FIFO
                                            // (occupying 16 bytes)
#define USB_FIFO_SZ_16_DB       0x00000012  // 16 byte double buffered FIFO
                                            // (occupying 32 bytes)
#define USB_FIFO_SZ_32_DB       0x00000013  // 32 byte double buffered FIFO
                                            // (occupying 64 bytes)
#define USB_FIFO_SZ_64_DB       0x00000014  // 64 byte double buffered FIFO
                                            // (occupying 128 bytes)
#define USB_FIFO_SZ_128_DB      0x00000015  // 128 byte double buffered FIFO
                                            // (occupying 256 bytes)
#define USB_FIFO_SZ_256_DB      0x00000016  // 256 byte double buffered FIFO
                                            // (occupying 512 bytes)
#define USB_FIFO_SZ_512_DB      0x00000017  // 512 byte double buffered FIFO
                                            // (occupying 1024 bytes)
#define USB_FIFO_SZ_1024_DB     0x00000018  // 1024 byte double buffered FIFO
                                            // (occupying 2048 bytes)
#define USB_FIFO_SZ_2048_DB     0x00000019  // 2048 byte double buffered FIFO
                                            // (occupying 4096 bytes)
#define USB_FIFO_SZ_4096_DB     0x00000020  //Biju

The value for 0x10 for 8192 should 0x0A. The values for the double buffering are all off by one. I think the correct defines should be:

#define USB_FIFO_SZ_8192        0x0000000A  // Biju

#define USB_FIFO_SZ_8_DB        0x00000010  // 8 byte double buffered FIFO
                                            // (occupying 16 bytes)
#define USB_FIFO_SZ_16_DB       0x00000011  // 16 byte double buffered FIFO
                                            // (occupying 32 bytes)
#define USB_FIFO_SZ_32_DB       0x00000012  // 32 byte double buffered FIFO
                                            // (occupying 64 bytes)
#define USB_FIFO_SZ_64_DB       0x00000013  // 64 byte double buffered FIFO
                                            // (occupying 128 bytes)
#define USB_FIFO_SZ_128_DB      0x00000014  // 128 byte double buffered FIFO
                                            // (occupying 256 bytes)
#define USB_FIFO_SZ_256_DB      0x00000015  // 256 byte double buffered FIFO
                                            // (occupying 512 bytes)
#define USB_FIFO_SZ_512_DB      0x00000016  // 512 byte double buffered FIFO
                                            // (occupying 1024 bytes)
#define USB_FIFO_SZ_1024_DB     0x00000017  // 1024 byte double buffered FIFO
                                            // (occupying 2048 bytes)
#define USB_FIFO_SZ_2048_DB     0x00000018  // 2048 byte double buffered FIFO
                                            // (occupying 4096 bytes)
#define USB_FIFO_SZ_4096_DB     0x00000019  //Biju

Questionable whether these defines should exist at all. They are used primarily as parameters to the USB_FIFO_SZ_TO_BYTES() macro. Why not just use the resultant values 8, 16, 32, ...?