Application: TMS320VC5509A works as a slave proccessor accessed by HPI from a ARM host in none-multiplexed mode.
The DSP use a 20MHz outside cristal,work on 200MHz freq. by inner PLL.
Problem:The system can work stablely on normal room temperature and on high temperature about 60 degree.
On low temperature(about -20 degree),the system can start normally,BUT can't run stable.some board crash in minutes,some crash in hours,there's only one board never crash.
I have a test to stop the HPI access from the ARM host,let the slave DSP run independly,the result is: Host and DSP both can run stable in -25 degree for a long time (about 16 hours test).
My design used a 1.6V LDO power chip to supply the DSP core according to the datasheet. I have a try to low down the core supply voltage to 1.5V,the system stability improved a lot,some board become never crash,some board can run longer time(from minutes to hours).
At last,I low down the core supply voltage to about 1.45V,and test all board for about 20 hours on -20 degree temperature,and all boards seem run OK.
I don't understand the theory and afraid of any hidden problem.
I am waiting for a answer urgently.
Thanks.