This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

not able to read RAW data from OV sensor

Hi all,

S/W Release version: IPNC_RDK_3.00

Platform: DM8127

               I received the IPNC setup that works well with the MT9J003 (12-bit RAW) sensor.

Looking to integrate OV sensor(10-bit RAW) to it. 

Assumed default ISIF / IPIPE_IF settings used for MT9J003 sensor works well with OV sensor as well.(since both are RAW sensors.)

Registers of OV are succesfully set using I2C.

By Enabling the DDR mode, now trying to read RAW data from CADU/CADL address. But data available here is '0'(ZERO) always...!! but I am looking for some RAW image...!!

Anyone knows the problem or possible solution??

Thanks in advance :)

Regards

Ravikiran