This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6437 EVM doesn't work

Other Parts Discussed in Thread: TMS320DM6437

I got a new TMS320DM6437 EVM. but it doesn't work. According to its simple Setup Guide it should work properly by default demo program which is loaded by the company on it.

Here is the steps I did:

1. I check the JP1, JP2 jumpers, also SW1, SW2, SW7 switch.

2. I connect the input video port to a video tape to simulate a live camera.

3. I connect the output video port to a TV

4. I turn on the board.

I expect to see the video tape on TV but it doesn't happen.

Why?

- Because I should load a Demo program on it by CCS?

- Because I should use real camera with specific resolution?

- Because my output port has problem?

I also tried to load a demo program on the board by CCS, the program successfully build with no errors and I load the program on the board successfully and run the demo from the Debug menu. Still no output

Please HELP!!