Dear all!
I have a question about Composite Device Drivers for OMAP L138. I am trying to create composite USB device with various drivers.
g_cdc works fine, but g_multi causes a error message like:
root@arago:~# modprobe g_multi host_addr=00:cc:cc:01:23:45 dev_addr=00:dd:dd:67:
89:ac file=/dev/mmcblk0p1 cdrom=0 ro=0 iSerialNumber=123456789
[ 52.165977] usb0: MAC 00:dd:dd:67:89:ac
[ 52.188269] usb0: HOST MAC 00:cc:cc:01:23:45
[ 52.229238] g_multi gadget: Mass Storage Function, version: 2009/09/11
[ 52.235850] g_multi gadget: Number of LUNs=1
[ 52.260155] lun0: LUN: removable file: /dev/mmcblk0p1
[ 52.288867] g_multi gadget: unable to autoconfigure all endpoints
[ 52.368501] netconsole: network logging stopped, interface usb0 unregistered
FATAL: Error inserting g_multi (/lib/modules/2.6.37/kernel/drivers/usb/gadget/g_multi.ko): Unknown error 524
I use DVSDK 4.00.03.06, kernel 2.6.37
Is it possible to use L138 in multifunction mode?