Hi,
I do develop on dm8168 evm board using dvrrdk 02.80. I read the dvrrdk mcfw_demo ,
In video capture , encode and display demo,
VcapVenc_bitsWriteCreate is used to create a thread to write 264 bitstream to hard disk.
In this demo CIF and mjpeg encode also is run, where these two bitstream saved then?
I don't see this part in VcapVenc_bitsWriteCreate function ?
when then ?