This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

which is the latest version surported to dm6467?

hi,

now i got a problem,when i turn on the target ,it blocked and show tips as follows:

Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (gzhxu@Redhat.localdomain) (gcc version 3.4.3 (MontaVista 3.4.3-25.0.104.0600975 2006-07-06)) #1 PREEMPT Fri Sep 14 15:15:07 CST 2012

CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177

Machine: DaVinci DM6467 EVM

Memory policy: ECC disabled, Data cache writeback

DaVinci DM6467 variant 0x0

CPU0: D VIVT write-back cache

CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets

CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets

Built 1 zonelists.  Total pages: 30720

Kernel command line: mem=120M console=ttyS0,115200n8 noinitrd rw ip=192.168.20.221:192.168.20.1:255.255.255.0 root=/dev/nfs nfsroot=192.168.20.101:/home/mnt/workdir/nfs,nolock davincihd_capture.channel0_numbuffers=4

PID hash table entries: 512 (order: 9, 2048 bytes)

......

NET: Registered protocol family 1

NET: Registered protocol family 17

drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

Time: timer0_1 clocksource has been installed.

Clock event device timer0_0 configured with caps set: 08

Switched to high resolution mode on CPU 0

above is the tips when it is running.

the sdk version i used is dvsdk_2_00_00_22 and target kernel is compiled from the '/mv_pro_5.0/montavista/pro/devkit/lsp/ti-davinci/linux-2.6.18_pro500 ' included in mv toos. 

what is the problem?anything else to be set ??

THX