This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issues on PRACH with C6670



Hi All,

I have noticed few issues while running the example PRACH code given by TI.

As per the release notes document  "Release Notes for 02.00.00 UMTS_LTE.pdf", in page 7, it says that, "A new function, LTELIB_cplxMac is now included to facilitate using the FFTC to extract the same 839 tones." But in the example code for PRACH Rx, the mentioned function is not being called at all. But i notice a seperate project with the same name. 

So do we have to include the both the projects to make the PRACH Rx work? or if there is any meachnism to test the PRACH Rx, if yes, please share the same.

Thanks in Advance

Regards

Lee