This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dm6437 encoder



hello ,

i'm developing an application based on h264 encode in dm6437,

i've problem in encoder, after capturing the video it encode for 10 to 20 frames

then it stop encoding but it is in running while i try to halt, it disconnect the board.

its happening for every time..

could anyone help me to solve problem?

  • hello ,

    i'm still facing the above problem . and following is my DVDP package.

    C:\dvsdk_1_01_00_15

                     biosutils_1_00_02

                     codec_engine_1_20_02

                     ndk_1_92_00_22_eval

                     psp_1_00_02_00

                     xdais_5_21

                     xdc_2_95_02

    i'm using the example/video_encdec code and this example showing error which we built,

    but it running in release mode which TI already provided.

    can any one help to solve problem?

    regards

    VS

  • waiting for the right answer.....