Hi All,
By inserting SIM card in HHT device, i am getting below msg for wvdial
/ # wvdialconf
Editing `/etc/wvdial.conf'.
Scanning your serial ports for a modem.
failed with 9600 baud, next try: 115200 baud
ttyS0<*1>: ATQ0 V1 E1 -- ttyS1<*1>: ATQ0 V1 E1 -- failed with 2400 baud, next td
ttyS1<*1>: ATQ0 V1 E1 -- failed with 9600 baud, next try: 115200 baud
ttyS1<*1>: ATQ0 V1 E1 -- and failed too at 115200, giving up.
ttyS2<*1>: ATQ0 V1 E1 -- failed with 2400 baud, next try: 9600 baud
ttyS2<*1>: ATQ0 V1 E1 -- failed with 9600 baud, next try: 115200 baud
ttyS2<*1>: ATQ0 V1 E1 -- OK
ttyS2<*1>: ATQ0 V1 E1 Z -- OK
ttyS2<*1>: ATQ0 V1 E1 S0=0 -- OK
ttyS2<*1>: ATQ0 V1 E1 S0=0 &C1 -- OK
ttyS2<*1>: ATQ0 V1 E1 S0=0 &C1 &D2 -- OK
ttyS2<*1>: ATQ0 V1 E1 S0=0 &C1 &D2 +FCLASS=0 -- OK
ttyS2<*1>: Modem Identifier: ATI -- ERROR
ttyS2<*1>: Speed 230400: AT -- Speed 230400: AT -- Speed 230400: AT -- Max spee.
ttyS2<*1>: ATQ0 V1 E1 S0=0 &C1 &D2 +FCLASS=0 -- OK
Found a modem on /dev/ttyS2.
Modem configuration written to /etc/wvdial.conf.
ttyS2<Info>: Speed 115200; init "ATQ0 V1 E1 S0=0 &C1 &D2 +FCLASS=0"
/ #
By inserting same SIM card in my Nokia mobile, i am getting below msg.
raghava@raghava-HCL-Notebook:/$ wvdialconf
Editing `/etc/wvdial.conf'.
Scanning your serial ports for a modem.
Modem Port Scan<*1>: S0 S1 S2 S3 S4 S5 S6 S7
Modem Port Scan<*1>: S8 S9 S10 S11 S12 S13 S14 S15
Modem Port Scan<*1>: S16 S17 S18 S19 S20 S21 S22 S23
Modem Port Scan<*1>: S24 S25 S26 S27 S28 S29 S30 S31
WvModem<*1>: Cannot get information for serial port.
ttyACM0<*1>: ATQ0 V1 E1 -- OK
ttyACM0<*1>: ATQ0 V1 E1 Z -- OK
ttyACM0<*1>: ATQ0 V1 E1 S0=0 -- OK
ttyACM0<*1>: ATQ0 V1 E1 S0=0 &C1 -- OK
ttyACM0<*1>: ATQ0 V1 E1 S0=0 &C1 &D2 -- OK
ttyACM0<*1>: ATQ0 V1 E1 S0=0 &C1 &D2 +FCLASS=0 -- OK
ttyACM0<*1>: Modem Identifier: ATI -- Nokia
ttyACM0<*1>: Speed 4800: AT -- OK
ttyACM0<*1>: Speed 9600: AT -- OK
ttyACM0<*1>: Speed 19200: AT -- OK
ttyACM0<*1>: Speed 38400: AT -- OK
ttyACM0<*1>: Speed 57600: AT -- OK
ttyACM0<*1>: Speed 115200: AT -- OK
ttyACM0<*1>: Speed 230400: AT -- OK
ttyACM0<*1>: Speed 460800: AT -- OK
ttyACM0<*1>: Max speed is 460800; that should be safe.
ttyACM0<*1>: ATQ0 V1 E1 S0=0 &C1 &D2 +FCLASS=0 -- OK
Found an USB modem on /dev/ttyACM0.
Modem configuration written to /etc/wvdial.conf.
/etc/wvdial.conf<Warn>: Can't write '/etc/wvdial.conf.tmp2736': Permission denied
/etc/wvdial.conf<Warn>: Can't write '/etc/wvdial.conf' ('/etc/wvdial.conf'): Bad file descriptor
ttyACM0<Info>: Speed 460800; init "ATQ0 V1 E1 S0=0 &C1 &D2 +FCLASS=0"
raghava@raghava-HCL-Notebook:/$
I per my knowledge HHT modem device not supporting for wvdial(modem is working fine but not supporting for wvdial).
I think need to develop script in our device to respond modem.
Pls suggest
Thanks Advance
Rgds,
Raghava,