Other Parts Discussed in Thread: TPS65217
Hi all, I'm using beagle bone rev A3 with Sitara sdk (version: ti-sdk-am335x-evm-05.05.00.00).
I need to uso the spi1 with my AD peripheral and I would like to access it at user level. As far I understood from the previous post ( http://e2e.ti.com/support/dsp/sitara_arm174_microprocessors/f/791/p/168122/699213.aspx#699213 ) I've to do it in two step:
1) modify the file board-am335xemv.c file I've added:
static struct spi_board_info am335x_spi1_slave_info[] = {
{
// .modalias = "m25p80",
.modalias = "spidev", //brt
.platform_data = &am335x_spi_flash,
.irq = -1,
.max_speed_hz = 1000000,
.bus_num = 2,
.chip_select = 0,
.mode = SPI_MODE_0,
},
};
/* Module pin mux for SPI flash */
static struct pinmux_config spi1_pin_mux[] = {
{"mcasp0_aclkx.spi1_sclk", OMAP_MUX_MODE3 | AM33XX_PULL_ENBL
| AM33XX_PIN_OUTPUT },
{"mcasp0_fsx.spi1_d0", OMAP_MUX_MODE3 | AM33XX_PULL_ENBL
| AM33XX_PULL_UP | AM33XX_PIN_OUTPUT },
{"mcasp0_axr0.spi1_d1", OMAP_MUX_MODE3 | AM33XX_PULL_ENBL
| AM33XX_INPUT_EN},
{"mcasp0_ahclkr.spi1_cs0", OMAP_MUX_MODE3 | AM33XX_PULL_ENBL
| AM33XX_PULL_UP | AM33XX_PIN_OUTPUT },
{NULL, 0},
};
/* setup bone spi1 */
static void bone_spi1_init(int evm_id, int profile)
{
pr_info("BRT:Beagle bone SPI init\n");
setup_pin_mux(spi1_pin_mux);
spi_register_board_info(am335x_spi1_slave_info,
ARRAY_SIZE(am335x_spi1_slave_info));
return;
}
/* Beaglebone Rev A3 and after */
static struct evm_dev_cfg beaglebone_dev_cfg[] = {
{tps65217_init, DEV_ON_BASEBOARD, PROFILE_NONE},
// {mii1_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{usb0_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{usb1_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{mmc0_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{i2c2_init, DEV_ON_BASEBOARD, PROFILE_NONE},
{bone_spi1_init,DEV_ON_BASEBOARD, PROFILE_NONE}, //brt
{NULL, 0, 0},
};
2) reconfigure the kernel to:
-enabling ==> User mode SPI device driver support (SPI_SPIDEV)
-disabling ==> McSPI driver for OMAP (SPI_OMAP24XX)
-disabling ==> Memory Technology Device (MTD) support (MTD)
I have successusfully recompiled the kernel and I was able to see sys files:
root@am335x-evm:~# find /sys -name "*spi*"
/sys/bus/spi
/sys/bus/spi/drivers/spidev
/sys/class/spi_master
/sys/class/spidev
/sys/module/spidev
But I cannot still found the /dev/spidev* devices...
Am I missing something? Where am I wrong?
Many thanks in advance
But still we ca