This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x TRM

Hi,

I just want to make sure that below is the statement I see in the AM335x TRM . http://www.ti.com/litv/pdf/spruh73f
 

 7.1.3.3.1 GPMC Clock Configuration
Table 7-6 describes the GPMC clocks.
:

:

GPMC_FCLK I Functional and interface clock
GPMC_CLK O External clock provided to synchronous external memory devices.
The GPMC_CLK is generated by the GPMC from the internal GPMC_FCLK clock. The source of the
GPMC_FCLK is described in . The GPMC_CLK is configured via the GPMC_CONFIG1_i[1-0]
GPMCFCLKDIVIDER field (for i = 0 to 3) as shown in Table 7-7.


Where is the description?

Best Regarts
Takao