Other Parts Discussed in Thread: OMAP-L137
I am trying to boot a DA830 REV A board that was shipped to me with U-Boot loaded without Linux. I was able to build DaVinci Linux and a root file system, and now I want to load Linux using tftp. I booted the board but am getting an error that "No ethernet was found.". Following is what the board starts up with:
SF: Detected W25Q32 with page size 4 KiB, total 4 MiB
In: serial
Out: serial
Err: serial
Net: Read from EEPROM @ 0x50 failed
Board Net Initialization Failed
No ethernet found.
U-Boot >
I found one forum that suggested that the ethernet address was not set, and I checked with:
U-Boot > env print ethaddr
ethaddr=FF:FF:FF:FF:FF:FF
And indeed it is not set. I attempted set it with the following and got an error:
U-Boot > setenv ethaddr 01:02:03:04:05:06
Can't overwrite "ethaddr"
I also attempted to set it with the following, but it still does not set:
U-Boot > env set -f ethaddr 01:02:03:04:05:06
U-Boot > env print ethaddr
ethaddr=FF:FF:FF:FF:FF:FF
I don't know what to try next. Maybe my switches aren't configured properly??