This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SCD performance in DVRRDK_03.00.00.00

Hello TI-friends,
 we found that there're two modules(LMD,DMVAL) inside SCD link. Basically, we just need LMD and I remark DMVAL-related function. And it works fine.
Now I increase the SCD input frame rate from 2 to 30. And I found that the frame rate could be 19~21 fps but the CPU loading is 60% around. Is there any way to improve the frame rate? because we need more sensitive LMD. Thanks.

here under are info by TI utility

 [c6xdsp ]  CH  | In Recv In Process User Skip Process Skip In Process Time
 [c6xdsp ]  Num | FPS     FPS        FPS       FPS          per frame (msec)
 [c6xdsp ]  ----------------------------------------------------------------
 [c6xdsp ]    0 |      21         21        0           0              1
 [c6xdsp ]    1 |      21         21        0           0              1
 [c6xdsp ]    2 |      21         21        0           0              1
 [c6xdsp ]    3 |      21         21        0           0              1
 [c6xdsp ]    4 |      21         21        0           0              1
 [c6xdsp ]    5 |      21         21        0           0              1
 [c6xdsp ]    6 |      21         21        0           0              1
 [c6xdsp ]    7 |      21         21        0           0              1
 [c6xdsp ]    8 |      21         21        0           0              1
 [c6xdsp ]    9 |      21         21        0           0              1
 [c6xdsp ]   10 |      21         21        0           0              1
 [c6xdsp ]   11 |      21         21        0           0              1
 [c6xdsp ]   12 |      21         21        0           0              1
 [c6xdsp ]   13 |      21         21        0           0              1
 [c6xdsp ]   14 |      21         21        0           0              1
 [c6xdsp ]   15 |      21         21        0           0              1

 [c6xdsp ]  2332331: LOAD: CPU: 58.4% HWI: 0.9%, SWI:0.4%
 [c6xdsp ]
 [c6xdsp ]  2332331: LOAD: TSK: IPC_FRAMES_IN1      : 0.6%
 [c6xdsp ]  2332331: LOAD: TSK: IPC_BITS_OUT1       : 1.0%
 [c6xdsp ]  2332331: LOAD: TSK: ALG1                : 3.2%
 [c6xdsp ]  2332331: LOAD: TSK: SCD_PROCESS_TSK1    : 49.9%
 [c6xdsp ]  2332331: LOAD: TSK: MISC                : 0.4%