Hi,
We are developing some other application like capture-encode, where the encoder component takes in the yuv4:2:0 progressive input.
So i have some queries on it.
1. Do we need to include dei module, as we want only single yuv 4:2:0 progressive input for encoder component.
2. if we include dei module, we get 2 sets of output in bypass mode (4:2:0 yuv and 4:2:2 yuv).
Actually we only require only one set of output, so please guide for setting the dei module only for single set of output.
Regards,
Sudeep