Other Parts Discussed in Thread: OMAP-L132
Hi,
Since the PRUs have only GPI/Os, I wonder if it is possible to implement using PRUs the communication interface with a peripheral that uses a bidirectional pin.
Thanks in advance,
Silvia
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L132
Hi,
Since the PRUs have only GPI/Os, I wonder if it is possible to implement using PRUs the communication interface with a peripheral that uses a bidirectional pin.
Thanks in advance,
Silvia
Hi Silvia,
Please mention the processor name, peripheral type and what are the PRU pins, you need to connect?
-Thanks,
Balaji N
Hi Balaji,
The processor is OMAP-L132, and the peripheral that I want to handle with the PRUs requires a 1-wire interface.
Thanks,
Silvia