This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6746 EMIFA Asynchronous Memory Write Operation Issue



Our customer has a issue.
It is that the order of Asynchronous Memory Write and GPIO Output is changed.

In the program code, the order as follows.

 1. 1st Memory Write
 2. 2nd Memory Write
 3. 3rd Memory Write
 4. 4th Memory Write
 5. GPIO Output is High

In The timing of the output signals, during the 1st Memory Write (CS is Low), GPIO Output becomes High.
I guess that it is because the DSP core does not wait for the Memory Write to be completed.

What should I do to fix this issue?

Best regards,

Daisuke