This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HELP!!!!Problem with start Android in pandaboard.



Anybody please help me, I used this manual http://omappedia.org/wiki/4AI.1.4_OMAP4_Icecream_Sandwich_Panda_Notes
for building android system and I finished this. But, when I input sdcard in pandaboard es, i have this error:

Texas Instruments Inc X-Loader 1.41.0 (Aug 15 2012 - 16:49:10)
OMAP4460: 1.2 GHz capable SOM
Starting OS Bootloader from MMC/SD1 ...


U-Boot 1.1.4 (Aug 15 2012 - 16:49:35)

Load address: 0x80e80000
DRAM: 1024 MB
Flash: 0 kB
Using default environment

In: serial
Out: serial
Err: serial

efi partition table:
256 128K xloader
512 256K bootloader
2048 8M recovery
18432 8M boot
34816 512M system
1083392 256M cache
1607680 1101M userdata
Net: KS8851SNL
Hit any key to stop autoboot: 0
kernel @ 80008000 (3184264)
ramdisk @ 81000000 (164844)
I2C read: I/O error

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Linux version 3.0.1-23108-g97cebce (lockwood@sirsasana.cam.corp.g
oogle.com) (gcc version 4.4.3 (GCC) ) #13 SMP PREEMPT Mon Aug 29 12:34:05 EDT 20
11
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387f
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

[ 0.000000] Machine: OMAP4 Panda board
[ 0.000000] Truncating RAM at 80000000-bfffffff to -afffffff (vmalloc region
overlap).
[ 0.000000] Reserving 20971520 bytes SDRAM for VRAM
[ 0.000000] Memory policy: ECC disabled, Data cache writealloc
[ 0.000000] OMAP4460 ES1.1
[ 0.000000] SRAM: Mapped pa 0x40300000 to va 0xfe400000 size: 0xd000
[ 0.000000] PERCPU: Embedded 7 pages/cpu @c0d91000 s6848 r8192 d13632 u32768
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pag
es: 188160
[ 0.000000] Kernel command line: console=ttyO2,115200n8 mem=1024M androidboot
.console=ttyO2 vram=20M omapfb.vram=0:16M androidboot.serialno=0146A5490E00E016
androidboot.bootloader=U-Boot_1.1.4
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 741MB = 741MB total
[ 0.000000] Memory: 743880k/743880k available, 42552k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
[ 0.000000] vmalloc : 0xf0800000 - 0xf8000000 ( 120 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .init : 0xc0008000 - 0xc0041000 ( 228 kB)
[ 0.000000] .text : 0xc0041000 - 0xc05ea000 (5796 kB)
[ 0.000000] .data : 0xc05ea000 - 0xc063e580 ( 338 kB)
[ 0.000000] .bss : 0xc063e5a4 - 0xc07866b0 (1313 kB)
[ 0.000000] SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=2, N
odes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] NR_IRQS:410
[ 0.000000] omap_hwmod: dpll_mpu_m2_ck: missing clockdomain for dpll_mpu_m2_c
k.
[ 0.000000] OMAP clockevent source: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 13
1071999ms
[ 0.000000] Calibrating delay loop... 1392.74 BogoMIPS (lpj=5439488)
[ 0.007873] pid_max: default: 32768 minimum: 301
[ 0.007873] Mount-cache hash table entries: 512
[ 0.071624] Initializing cgroup subsys debug
[ 0.071624] Initializing cgroup subsys cpuacct
[ 0.071716] Initializing cgroup subsys freezer
[ 0.071777] CPU: Testing write buffer coherency: ok
[ 0.071960] twd_timer_setup: no clock found
[ 0.071960] Calibrating local timer... 341.51MHz.
[ 0.117431] L310 cache controller enabled
[ 0.117431] l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x5e470000, Cache si
ze: 1048576 B
[ 0.193695] CPU1: Booted secondary processor

...

...

...

Reprogramming LPDDR2 timings to 400000000 Hz
[ 6.780731] Power Management for TI OMAP4.
[ 6.785308] OMAP4 PM: Static dependency added between MPUSS <-> EMIF MPUSS <-
> L4_PER/CFG and MPUSS <-> L3_MAIN_1.
[ 6.831390] mmc0: host does not support reading read-only switch. assuming wr
ite-enable.
[ 6.839996] mmc0: new SD card at address aaaa
[ 6.845062] mmcblk0: mmc0:aaaa SD02G 1.84 GiB
[ 6.857238] Alternate GPT is invalid, using primary GPT.
[ 6.862976] mmcblk0: p1 p2 p3 p4 p5 p6 p7
[ 6.867462] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 6.876586] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 6.883422] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1317000 v
olt
[ 6.891265] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=92
0000000, v=1317000]
[ 6.900695] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 6.910064] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 6.916931] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1025000 v
olt
[ 6.924743] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=35
0000000, v=1025000]
[ 6.934295] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 6.941772] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 6.950256] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1380000 v
olt
[ 6.952209] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=12
00000000, v=1380000]
[ 6.968231] cannot apply mgr(lcd) on inactive device
[ 6.968322] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 6.968353] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 6.968353] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1380000 v
olt
[ 6.968383] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=12
00000000, v=1380000]
[ 7.006652] omapfb omapfb: failed to apply dispc config
[ 7.015228] cannot apply mgr(tv) on inactive device
[ 7.020446] omapfb omapfb: failed to apply dispc config
[ 7.028991] cannot apply mgr(lcd2) on inactive device
[ 7.034423] omapfb omapfb: failed to apply dispc config
[ 7.043029] omapdss DPI: Could not find exact pixel clock. Requested 74250 kH
z, got 76800 kHz
[ 7.054687] regulator_init_complete: VANA: incomplete constraints, leaving on

[ 7.062255] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 7.071441] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 7.078308] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1025000 v
olt
[ 7.086242] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=35
0000000, v=1025000]
[ 7.095703] regulator_init_complete: CLK32KG: incomplete constraints, leaving
on
[ 7.104797] regulator_init_complete: VDAC: incomplete constraints, leaving on

[ 7.112823] regulator_init_complete: VCXIO: incomplete constraints, leaving o
n
[ 7.121520] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
[ 7.128448] Freeing init memory: 228K
[ 7.135650] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_s
core_adj instead.
[ 7.168334] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 7.179168] usb 1-1.1: new high speed USB device number 3 using ehci-omap
[ 7.187164] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 7.194183] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1317000 v
olt
[ 7.217254] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=92
0000000, v=1317000]
[ 7.249023] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 7.258148] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 7.258148] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1380000 v
olt
[ 7.272857] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=12
00000000, v=1380000]
[ 7.312164] usb 1-1.1: New USB device found, idVendor=0424, idProduct=ec00
[ 7.320312] usb 1-1.1: New USB device strings: Mfr=0, Product=0, SerialNumber
=0
[ 7.330963] smsc95xx v1.0.4
[ 7.347381] EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. O
pts: (null)
[ 7.381835] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 7.391021] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 7.398284] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1025000 v
olt
[ 7.406524] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=35
0000000, v=1025000]
[ 7.416076] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 7.425811] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 7.432739] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1025000 v
olt
[ 7.441101] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=35
0000000, v=1025000]
[ 7.446166] smsc95xx 1-1.1:1.0: eth0: register 'smsc95xx' at usb-ehci-omap.0-
1.1, smsc95xx USB 2.0 Ethernet, 2e:3d:fb:66:65:07
[ 7.462829] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 7.471954] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 7.478790] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1380000 v
olt
[ 7.483306] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=12
00000000, v=1380000]
[ 7.591430] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 7.591430] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 7.607360] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1025000 v
olt
[ 7.615386] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=35
0000000, v=1025000]
[ 7.624938] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 7.624938] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 7.640899] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1380000 v
olt
[ 7.647277] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=12
00000000, v=1380000]
[ 7.749389] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 7.758544] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 7.765380] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1025000 v
olt
[ 7.773223] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=35
0000000, v=1025000]
[ 7.782745] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 7.792022] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 7.798858] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1380000 v
olt
[ 7.806732] platform mpu.0: omap_device_scale: scale by mpu.0 failed -61[f=12
00000000, v=1380000]
[ 7.897583] omap_vp_get_curr_volt: PMIC function to convert vsel to voltagein
uV not registerd
[ 7.905090] voltdm_scale: No voltage scale API registered for vdd_mpu
[ 7.913543] platform mpu.0: _dvfs_scale: Unable to scale the mpu to 1025000 v
olt and etc.....