Hi All,
I am using AM1808 which is running the file system over SD-Card. I have configured the Mini USB driver as mass storage as device.
When i am connecting this AM1808 device to computer in Linux it shows "Linux File-CD Gadget". But is not accesing the drive.
If it is connecting in Windows it shows as mass storage, but it is not shoing any files and no drive.
My main intention is to connect to AM1808 device with WINDOS PC using USB mini cable and dump required files without open SD-Card.
How the files are copying in Mobile. the same way i am looking. Could please solve my issue.
Regards,
Franci