This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM814x no console output when attempting to boot from SD card

I am attempting to boot the demo application from the SD card.  This had previously worked a few months ago, then the board was placed back into the box until today.  The demo application does not boot, and I do not receive a TI-MIN# prompt in minicom.  My settings are as follows:

SW1:  111010000000

SW2:  10

Minicom:  115.2k, 8n1 no flow control

I have tested my cables on other equipment and they are working.  Is this board dead?