Hi, is just that i did a connection by I2C between the DS1307 RTC module and a pandaboard based on OMAP4430, and it is connected to level shifters for the connection with the pandaboard, i did activate the driver in the kernel for it, but i don't see any change, is there any other configuration that must be done to make it work????, please help, i need to have this done really soon, and i don't know what else must be configured. I'm using Android ICS and kernel 3.0.8. Thanks in advanced.
Best Regards.