Other Parts Discussed in Thread: TWL6040, 4460
Hi,
I want to connect external audio codec to Pandaboard. But there is no any I2S signals available on external header of Panada board. So i decided
to use PCM signals. TPs are available on this signals on Panda board and also these are multiplex with McBSP3 signals.
Now PCM signals are connected with Audio Phonix IC TWL6040. If i want to use this signals then I need to power down the Audio IC or put it in Reset. As I can not put it
in reset because it uses common reset singal of panda board. So I have only one option is , Power down the Audio IC.B y putting "AUDPWRON" signal in low mode Audio codec will go in power down.
Can anybody tell me that my thought and connection is right or not ?
Please see attached snap what connections I prepared. Please check and let me know my connection work or not ?
Thanks,
Hitesh Gambhava