Other Parts Discussed in Thread: OMAP-L138
Hello,
i need to choose one of the DSP micros. The questions is which one? I need to help.
It will be aplication, in which i want to use ADC for sampling data, then i will follow with filtering and DAC for outup. The signal will be in range of 20- 20kHz. It doesnt needs to be low power,but i "normal" package :D Im able to solder QFN, but PQFP, or something similar will be better. Maybe SPI driver will suited.
Thank you a lot, im lost in all the parametres:)