This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ecap and beaglebone starterware

I want to make a sample code about ecap 0 in starterware with beaglebone , please give me the steps for configuration 

Thanks and Best Regards

  • Hi do minh quoc,

    Ecap cab be used for  capturing input events and also to generate PWM output. The starterware package has sample code for generation of PWM output. It can found in examples/evmAM335x/demo/demoEcap.c file. Do you want sample code for PWM output or for capturing the input events?.

    Regards                                                                                                                                                                                                                                                                                             

  • i want sample code for capture event , the starterware have just a pwm code, I make two file for capture event , please check for me6215.capture.zip

    Regards