This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB mounting error (usbfs: interface 0 claimed by usbfs whi le 'xxx' sets config #1)

Hi 
I'm working with android and using Linux kernel 3.2 ( rowboat-am335x-kernel-3.2 ).
I trying to use my finger print scanner service with android, the scanner communicate over USB.
so i have add the libusb.so and libusb1.0.so into the system/lib folder manually.
Then i have mount the usb manually in init.rc with this line " mount usbfs none /proc/bus/usb -o devmode=0666 "  
Then i have add the service file into system/bin/sensor-service, and i have edit the init.rc with this line 

service sensor-service /system/bin/sensor-service
                 oneshot
                 disable
on property : persist.service.sensor.enable=1
                 start sensor-service
on property : persist.service.sensor.enable=0
                      stop sensor-service

When i booting my device and enable the service by setprop.persist.service.sensor.enable 1, i got the following error  
                     

root@android:/ # [ 315.569427] usb 1-1: usbfs: interface 0 claimed by usbfs while 'sensor-Service' sets config #1
[ 315.578582] usb 1-1: usbfs: interface 0 claimed by usbfs while 'sensor-Service' sets config

where i did the mistake, or any prob in mounting ? 

can any one have idea to fix it ?

Thanks in advance