This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X- Debugging problem

Hi,

I'm using AM335x-Starter kit and I have problem in loading the Starterware Demo into the target board.

After configuring the CortxA8 target with ti\AM335X_StarterWare_02_00_00_06\tools\gel\AM335x.gel, when I try to load the starterware demo application, I'm getting the following error.

"M3_wakeupSS_1: Error connecting to the target: (Error -1266 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.0.791.0)"

I don't have the SD card in the board, but still I cannot connect to the target

Any help is appreciated!

Thanks and Regards,

Easwar